| Site Search | Product Search | IA Global Search |
...the type of error. Temperature Sensor type Temperature Sensor error Control output Thermocouple input Burnout OFF Short-circuit ON if the set point is higher that the temperature at the short...
...oltage E5C4-Q40[] E5CS-Q[] See note 3 Note: 1.The [] in E5C4 model number indicates the type of input temperature sensor. It is "K" for the CA Thermocouple, "J" for the IC Thermocouple, and "...
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...
...r output for a humidity of 0% to 100%. Select a Temperature Controller that supports a 1 to 5-V input, and set the input range to 1 to 5 V for the Controller. Connectable Controllers...
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...
...t capacity for the number of Sensors connected. Example: S8VS-01524 Switch Mode Power Supplies (Input: 100 to 240 VAC, Output: 24 VDC, 0.65 A) S82K-00324 Switch Mode Power Supplies (...
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...
... the zero point, the phases must be the same. Phase difference may result in malfunctions. (The input signal and output amount will not match.) MY Best-selling, general-purpose relays that ca...
... constant-current circuit functions to automatically regulate to the current in response to the input signal. Inrush current is suppressed by reducing the ON phase. (Overcurrent detection wil...
...n the Displacement Sensor (analog signal output 4-20mA) and the Digital Panel Meter (DC voltage input type) *It is required that the connecting resistance value is within the allowable load r...
...ode 1 (rotational/circumferential speed) is ±0.006% rdg ±1 digit. If the variation of input pulses is not considered, the error depends on the number of significant digits displayed...
...onnect two Meters. Connect the Meters in parallel, as shown in the following diagram. Note: The input resistance of the K3NX and K3TS is 10 Ω. When connecting two K3NX or K3TS Process Meters,...
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...
...wer supply −). Note:The FM output from a Mitsubishi inverter is a voltage pulse output. NB: NPN input or voltage pulse input connections PB: PNP input connection NPN open-co...
...m fluctuating due to significantly fluctuating analog inputs or reducing the effect of noise in input signals that contain noise. The following chart shows the display when average processing...
...related to the previous average. This function can eliminate periodic noise superimposed on the input signal. The number of samples can be selected for the moving average. In the K3HB-X, K3HB...
...gital Panel Meter after checking the power voltage and current. 2. In the case of Analog Signal Input Applicable Digital Panel Meter K3HB-X, K3HB-V, K3HB-S, K3GN, K3MA-J, K3TE, K3TF 3. In the...
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...