Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 241 - 26026275
FAQ01847 for Power Controllers | OMRON Industrial ...

...? Answer  No. Three-phase loads are controlled by each having a phase angle separated by 120°, so three G3PX Units for single-phase applications cannot be used. Always use a Three-phase Cont...

https://www.ia.omron.com/support/faq/answer/54/faq01847/

FAQ01272 for Ultrasonic Sensors | OMRON Industrial...

...cation, use the E4R-SP Pulse Unit. The pulses generated by the E4R-SP synchronizes the Sensors, so up to ten E4R-2 Sensors can be used for synchronous operation without malfunction due to int...

https://www.ia.omron.com/support/faq/answer/50/faq01272/

Safety use of Rotary Encoders | OMRON Industrial A...

...ing is correct. Incorrect wiring may explosion or burning. Do not short-circuit the load. Doing so may cause explosion or burning. Make sure the power is OFF before performing wiring work. If...

https://www.ia.omron.com/product/cautions/52/precautions_for_safety_use.html

Thermal Condition Monitoring Tool software | OMRON...

...jects surrounding us, including industrial goods, architecture, software, systems, services and so on. The G Mark, as proof of winning GOOD DESIGN AWARD, is widely popular with consumers with...

https://www.ia.omron.com/product/special/fhv7_design/

Sysmac Library downloads | OMRON Industrial Automa...

... associated media, printed materials such as manuals, "online" or electronic documentation, and so on. LICENSE AGREEMENT OMRON grants the User a non-exclusive and limited license to use this ...

https://www.ia.omron.com/product/tool/sysmac-library/

E4PA-N Ultrasonic Displacement Sensor/Features | O...

...he 0.5-m type, a repeat accuracy of 1 mm or better has been achieved. The Sensor is ultrasonic, so it is not affected by the color of objects. A variety of materials can be measured, includin...

https://www.ia.omron.com/products/family/1467/

TP70 On-site Flexible Rod Switch/Features | OMRON ...

...plastic rod actuator makes the Switch easy on hands. • One-way operation: Equipped with stopper so that operation is only possible from one direction. • Distinctive yellow used for the body. ...

https://www.ia.omron.com/products/family/304/

FJ Series (Camera and Software Vision Package) PC ...

... easily. It allow you to edit the program on the controller and the compiling is not necessary. So you can develop and adjust the system quickly. ・Microsoft® Visual Studio® and Windows are ei...

https://www.ia.omron.com/products/family/3069/

FH-SMD 3D Robot Vision System/Features | OMRON Ind...

...etect parts inside the bin. To detect these parts, an operator must reposition items in the bin so that the parts are within the field of view. Cameras installed at the robot arms can reduce ...

https://www.ia.omron.com/products/family/3827/

iPF Series Flexible Part Feeder/Features | OMRON I...

...asic applications. CAD models of the hopper and feeder can be integrated into the ACE platform, so parts will be manipulated as expected every time. This simple integration process reduces de...

https://www.ia.omron.com/products/family/3907/

Y92[] Accessories/Features | OMRON Industrial Auto...

...e Sensor. Sputter Protective Covers (Threaded on Inside of Cover) • The cover uses Fluororesin, so that chips that adhere due to sputtering can be easily removed. Sputter Protective Covers (N...

https://www.ia.omron.com/products/family/484/

CS Series Programmable Controllers/Features | OMRO...

...e active CPU Unit, the standby CPU Unit takes over in an instant (using the hot standby method) so that system operation continues essentially unaffected. Other duplex variations are also pos...

https://www.ia.omron.com/products/family/9/

Overview of Push Buttons / Indicator Lamps Technic...

...Operating Action Terms for Configuration and Structure A Pushbutton Switch is a switch designed so that its contacts are opened and closed by depressing and releasing a pushbutton on the Swit...

https://www.ia.omron.com/support/guide/38/overview.html

introduction.html

...M control. The inverter outputs a pulsed voltage, and the pulses are smoothed by the motor coil so that a sine wave current flows to the motor to control the speed and torque of the motor. Th...

https://www.ia.omron.com/support/guide/9/introduction.html

Country-specific Radio Regulations of RFID Equipme...

...orm to the regulations on radio equipment of that country. We have obtained type approvals etc. so that OMRON products can be used in the following countries. Be aware that OMRON RFID equipme...

https://www.ia.omron.com/support/models/rfid/

Efforts to Comply with the RoHS Directive | OMRON ...

... other electrical and electronic equipment for use. Our finished products fall into category 9, so they are exempt from the RoHS Directive as of April 2007. Products such as sensors that are ...

https://www.ia.omron.com/support/models/rohs/

The Correct Fan Must Be Selected to Prevent Failur...

...the total heating value. Generally speaking, the heating value indicates the power consumption, so you can assume that the power consumption equals the heating value. Heating value(W) = In...

https://www.omron.com.tw/solution/panel/article/article_000821.html

NX-series Safety Controllers / Safety Network Cont...

...ra-high-speed machine automation - Bring safety to your production site Safety I/O Unit NX-SI / SO Build a simple and flexible safety system...

https://www.ia.omron.com/products/category/safety-components/safety-controllers/nx-series-safety-controllers_safety-network-controllers/

FAQ02315 for Safety Limit Switches | OMRON Industr...

...le interlocking components, related to the direct opening mechanism (forcibly opened contacts), so that the components will not distort or come apart even if great force is applied to the Act...

https://www.ia.omron.com/support/faq/answer/31/faq02315/

FAQ00828 for Digital Panel Indicators | OMRON Indu...

...value until n samples have been measured. The displayed value is just the average of n samples, so the previous set of data is unrelated. This function is useful when you want to lengthen the...

https://www.ia.omron.com/support/faq/answer/62/faq00828/

結果 241 - 26026275

国/地域選択

Related Contents