| IAグローバル検索 |
...w beam diameter of minimum 2.5 mm The E3S-DB has a response time of 0.5 ms for a pitch of 5 mm, so detection is possible at a conveyor speed of up to 4 m/s. (With the E3S-DB[][]2(T) and a sen...
... Optical Axis Accuracy The offset between the optical axis and mechanical axis is within ±2.5°, so a sufficient incident level can be achieved merely by aligning the mechanical axis at instal...
...use it’s easier to aim at the desired terminal. Safety The structure provides finger protection so that your fingers never touch conductive parts. Minimum Width of 3.5 mm to Help Downsize Con...
... Characteristics and Reinforced Insulation for Safety Standard Compliance UL-listed components, so you can reduce the time required for the UL application process. • Using new components or u...
...egistration, RCM, cULus Simplicity improves reliability Unnecessary complexity causes problems, so we’ve eliminated it totally, to improve reliability, maximize performance. • No internal cab...
...egistration, RCM, cULus Simplicity improves reliability Unnecessary complexity causes problems, so we’ve eliminated it totally, to improve reliability, maximize performance. • No internal cab...
...atility and range of Windows programs. The two platforms operate simultaneously but separately, so if Windows is down, the machine just keeps on working. As a result, engineers become unstopp...
...in the status which will have an effect on quality and to automatically control the temperature so that the optimal state is always maintained, in the same way as a skilled worker would. This...
...in the status which will have an effect on quality and to automatically control the temperature so that the optimal state is always maintained, in the same way as a skilled worker would. This...
...and acts as a beacon to help the robot navigate. The robot uses a Landmark as a reference point so it can better locate objects within the workspace. During high-mix, low-volume production wi...
...ase of the shutter. Easy filter replacement The light cover and optical filter are replaceable, so you don't need to prepare a protection cover against dirt. Single camera for inspecting vari...
... which allows multiple input voltage ranging 100 to 240 VAC. Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...
...te: May 6, 2021 For less design effort DC Axial Fans R89F-DS Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...
...oducts with safety outputs of which voltage, current, and power are limited to a certain level, so that not to cause an electric shock or fire,” and is evaluated by UL1310. For the UL Class 2...
...etect parts inside the bin. To detect these parts, an operator must reposition items in the bin so that the parts are within the field of view. Cameras installed at the robot arms can reduce ...
...ate of change of the heater resistance value and monitor the state and tendency of each heater, so it is possible to determine when replacement is necessary, so it is unplanned while...
...asic applications. CAD models of the hopper and feeder can be integrated into the ACE platform, so parts will be manipulated as expected every time. This simple integration process reduces de...
...imed STO. The torque in the motor is removed at a certain (settable) time after SS1 activation, so the controller has time to stop the load in a controlled manner before the STO is executed. ...
...etup completed in just a few minutes Intuitive UI for effortless use The AI Detection Camera is so intuitive that even first-time users can set it up. Just follow the on-screen steps and conf...
...le and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, so we can grow with your business. Grow Your Business − Modify layouts to optimize production A...