| IAグローバル検索 |
... associated media, printed materials such as manuals, "online" or electronic documentation, and so on. LICENSE AGREEMENT OMRON grants the User a non-exclusive and limited license to use this ...
https://www.ia.omron.com/product/tool/ipc-machine-controller/index.htm
... ZX-GTC41 Accessories (Order Separately) These are not included with the sensor and controller, so order these accessories separately if necessary. Set: Interface Unit (RS-232C/Binary output)...
...ing Bracket: Tilt the Sensor Head towards the workpiece as shown below. Adjust the installation so that the angle is 10.5° ±0.1°. * The mounting hole dimensions in parentheses (reference valu...
https://www.ia.omron.com/products/family/2979/dimension.html
...nutes to seconds Result of Learn • Tools arranged in reading order • ROIs (Regions of Interest) so each code can be read uniquely • ROI sized to accommodate the expected positional uncertaint...
...ndards. When the quality of the barcode printing is not good, the data may be read incorrectly, so it is important to take care in printing labels etc. Features of Barcodes Highly flexibility...
...ions with Host Devices Ethernet Connection The compact body also provides an Ethernet connector so that you can transfer read data and images via Ethernet. Smoothly transfer data to PLCs, com...
...In a machine operation intervention such as removing a crashed product, the machine is stopped, so there is no production. SOLUTION • You can pickup the product safely with Safely-Limited Spe...
...t harmonics. The W-series Servomotors are equipped with a terminal connection for a DC Reactor, so a DC Reactor can be connected. OMRON offers Reactors to control harmonics in other Servomoto...
... associated media, printed materials such as manuals, "online" or electronic documentation, and so on. LICENSE AGREEMENT OMRON grants the User a non-exclusive and limited license to use this ...
https://www.ia.omron.com/product/tool/h5cc_calculation/index.htm
...mple data, associated media, printed materials such as manuals or electronic documentation, and so on. LICENSE GRANTED OMRON grants the User a non-exclusive and limited license to use the Sof...
...tch a standard load, it cannot be used for a load of a smaller capacity. Doing so may result in roughening of the contact surface and contact reliability may be lost. *1. The...
https://www.ia.omron.com/products/family/1497/specification.html
...k Connection error will occur. Set the pulse width of signals input to the Interrupt Input Unit so they satisfy the following conditions. The signal names of the terminals are the device vari...
https://www.ia.omron.com/products/family/1642/specification.html
...ecting Socket P3GA-11 Back Connecting Socket Note: Do not use any other types of Sockets. Doing so will adversely affect the accuracy. Applicable Thermistors Use Element Interchangeable Therm...
...(W267) for the communications power supply specifications. *2. The Device Unit uses a node, and so connection is possible to 63 slaves only. *3. When the DeviceNet is used as a slave, "input"...
https://www.ia.omron.com/products/family/28/specification.html
...2F-45 Adapter. To use the USB- Serial Conversion Cable to make the settings, do so before you mount the Temperature Controller in the panel. 4. You cannot use this ...
https://www.ia.omron.com/products/family/3024/dimension.html
...ed in JIS K 2241:2000; Temperature: 35 °C max.) *2. The optical fiber is 2 m long on each side, so the sensing distance is 4,000 mm. Note: 1. The following mode names and response times apply...
...000 * HS: 3,450 ST: 4,000 * SHS: 920 E32-LT11R 2M * The optical fiber is 2 m long on each side, so the sensing distance is 4,000 mm. Note 1.The following mode names and response times apply t...
...d iris adjustment may become loose or come off due to shock or vibration during transportation, so please be caution when unpacking. last update: March 10, 2025...
...t be bent. 3. Do not use in locations subject to excessive vibration and shock. Doing so may cause disconnection. E52-CA6F-N-25 Note: 1. The thermocouple is a single wire from the t...
https://www.ia.omron.com/products/family/3151/dimension.html
... SHS: Super-high-speed mode (30 μs) *2. The optical fiber is 2 m long on each side, so the sensing distance is 4,000 mm. *3. The values for the minimum sensing object are referenc...