Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 641 - 66026275
FAQ00653 for Temperature Controllers | OMRON Indus...

... over a controlled object would be difficult if heating was the only type of control available, so cooling control was also added. Two control outputs (one for heating and one for cooling) ca...

https://www.ia.omron.com/support/faq/answer/53/faq00653/

FAQ01870 for Power Controllers | OMRON Industrial ...

...ks, thereby extending the service life of the heater. 3.The gradient can be set as desired, and so the output amount can be set when a Power Controller is used in a set with a Temperature Con...

https://www.ia.omron.com/support/faq/answer/54/faq01870/

FAQ01992 for Power Controllers | OMRON Industrial ...

...t is less than 1A, decrease in output signals cannot make output elements keep in the ON state, so that oscillating waveform may occur or they may not be turned ON. MY Best-selling, general-p...

https://www.ia.omron.com/support/faq/answer/54/faq01992/

faq00502

...ween the HIGH threshold value and the LOW threshold value is smaller than the hysteresis value, so that a PASS judgment is not possible. The setting is thus not allowed. Remedy 2: Make the hy...

https://www.ia.omron.com/support/faq/answer/56/faq00502/

faq01222

...ge remains the same until the next nth sampling is taken. It is simply the average of n samples so it has nothing to do with the previous data. The output response is slower for simple averag...

https://www.ia.omron.com/support/faq/answer/56/faq01222/

faq01289

...hicle on expressway, motorcycle and etc.) 3. High-temperature objects Surrounding air is heated so that ultrasonic waves may be reflected. E2E Standard Sensors for Detecting Ferrous Metals un...

https://www.ia.omron.com/support/faq/answer/56/faq01289/

faq01307

...y the other three settings as described above. The effectiveness depends on the sensing object, so always confirm operation with the actual system. E2E Standard Sensors for Detecting Ferrous ...

https://www.ia.omron.com/support/faq/answer/56/faq01307/

faq01335

...ure compensation function makes it easy to set the measurement range. The Sensor is ultrasonic, so it is not affected by the color of objects. Perform a variety of control operations by combi...

https://www.ia.omron.com/support/faq/answer/56/faq01335/

faq01356

...fect E4PA Ultrasonic Sensor? Answer  The Ultrasonic Switch uses air as the translation medium, so it is easily affected by wind. Care must be taken when using this Sensor but the E4PA is the...

https://www.ia.omron.com/support/faq/answer/56/faq01356/

faq03137

...ll appear instead of the warming-up display. Warming up itself, however, will not be completed, so high-accuracy measurements will not be possible. Also, ZX-L-N Laser type does not have this ...

https://www.ia.omron.com/support/faq/answer/56/faq03137/

faq03167

...r's Measurement Head of D5V cannot be replaced. The Flat Actuator, D5V[]-3F1, has an M2.5 screw so the Measurement Head can be replaced. Models that have a replaceable Measurement Head are th...

https://www.ia.omron.com/support/faq/answer/56/faq03167/

faq03292

... above 1 μm. Heat rays emitted from the hot object are similar in wavelength to the laser beam, so the receiver element may detect the heat rays. Conduct tests with the actual system to deter...

https://www.ia.omron.com/support/faq/answer/56/faq03292/

FAQ02453 for Emergency Stop Switches | OMRON Indus...

... the Operation Unit or the Socket Unit. The lever has a hole with an inside diameter of 6.5 mm, so the lever can be moved in the specified direction by inserting a screwdriver into the hole a...

https://www.ia.omron.com/support/faq/answer/60/faq02453/

faq02462

...Extractor. 2.Mounting the LED The following figure shows the mounting direction. Insert the LED so that the protrusions on the LED line up with the narrow guides on the socket unit. 3.Mountin...

https://www.ia.omron.com/support/faq/answer/60/faq02462/

FAQ00705 for Digital Panel Indicators | OMRON Indu...

...m/h × (0.006%) = ±0.0051 km/h In this case, three digits are displayed below the decimal point, so the fourth digit below the decimal point in ±0.0051 km/h is rounded off to yield an accuracy...

https://www.ia.omron.com/support/faq/answer/62/faq00705/

FAQ01729 for Measuring / Motor Protective Relays |...

...swer  The CT has specific wiring and the Power Sensor has polarity (see Figure 1). Wire the CT so that the load side of the sensing line is on the side of the CT with the label "L" and the p...

https://www.ia.omron.com/support/faq/answer/65/faq01729/

faq03062

...lays operating the instant that an overcurrent is detected. A starting current flows in motors, so Relays do not operate for a certain time during startup and then switches to instantaneous r...

https://www.ia.omron.com/support/faq/answer/65/faq03062/

faq04290

...90 Related Contents Primary Contents Question ZEN Programmable Relays: How do I write a program so that the coil turns ON for only one cycle when the power is turned ON? Answer  See the prog...

https://www.ia.omron.com/support/faq/answer/66/faq04290/

faq04299

...99 Related Contents Primary Contents Question ZEN Programmable Relays: How do I write a program so that the coil turns ON for only one cycle when the contact turns OFF? (downward differentiat...

https://www.ia.omron.com/support/faq/answer/66/faq04299/

faq04304

...04 Related Contents Primary Contents Question ZEN Programmable Relays: How do I write a program so that the coil turns ON for only one cycle when the contact turns ON? (upward differentiation...

https://www.ia.omron.com/support/faq/answer/66/faq04304/

結果 641 - 66026275

国/地域選択

Related Contents