| IAグローバル検索 |
...igures, there is no problem if the magnet section (GLS-M1) is rotated 180°. However, install it so that the direction of travel is in the direction of the arrow. The sensing distance will dec...
...ber of Sensors used increases the probability of oscillating frequencies coming close together, so mount the Sensors at distances of at least the catalog values. E2E Standard Sensors for Dete...
...e following characteristics: Internal electronic components are placed in the amplifier section so that they are not subjected to high temperatures. Heat-resistant parts are used for the case...
...igure 1, the surface of the detection coil on Shielded Proximity Sensors is covered with metal, so the flux is concentrated at the front of Sensors, which reduces the influence of surrounding...
...collector output is used, current will flow to F92A in one direction, as shown in Figure 2, and so the change in impedance input to Proximity Sensors will be reduced by half. To obtain the sa...
...ectrostatic capacitance will also change when the status of the electrical load is changed, and so stable detection cannot be performed. For stable detection, it is recommended to first ioniz...
...se make the hole of the same size as the lens diameter basically. Please refer to the following so that the idea is different depending on the sensing method. 1. Idea to use the light through...
...dual photodiode through a light receiving lens. The position of the dual photodiode is adjusted so that N side and F side of the dual photodiode become the same amount of receiving light, and...
...ill make it impossible to detect the object. The light will not be polarized at the object, and so the polarizing filter at the light-receiving side will prevent the reflected light from bein...
...of the illuminance is approx. 10,000 lx max in shade. This value is changed the sunlight power. So, the value is just for your reference. E2E Standard Sensors for Detecting Ferrous Metals und...
...S Reflectors? Answer E39-R1S has better reflection efficiency and directionality than E39-R1, so more light returns to the receiver, which enables a longer sensing distance. For reference, ...
...d how can it be corrected? Answer Retroreflective Sensors normally have the MSR function, and so shiny sensing objects can also be detected. Perform a test before using Sensors for sensing ...
.... Does voltage need to be applied to both of these? Answer No. They are internally connected, so only one of them needs to be powered. Applicable models: M7E-08,M7E-12, M7E-20, and M7F Digi...
...r of these happens, vibrations similar to earthquakes are probably being detected in that area, so change the installation location. E2E Standard Sensors for Detecting Ferrous Metals under St...
...dicator (red LED) will begin to flash. Countermeasure: Place the Sensors apart from one another so that they do not interfere with each other. E2E Standard Sensors for Detecting Ferrous Metal...
...ure compensation function makes it easy to set the measurement range. The Sensor is ultrasonic, so it is not affected by the color of objects. Perform a variety of control operations by combi...
...edium. In normal atmosphere, reflection from any object (even human bodies) is well transmitted so detection of that object is easy. E2E Standard Sensors for Detecting Ferrous Metals under St...
...re changed. (2) Correcting PID constants when there is external disturbances in the temperature so that the temperature falls within a specified range. (3) Correcting PID constants when hunti...
...h. The extension will cause the resistance of the lead wires to affect the display temperature, so use lead wires with thick conductors. (OMRON does not carry lead wires for extension. Use co...
...it set on the E5[]N? Answer 1. Direct/Reverse Operation (1) Direct operation performs control so that the manipulated variable is increased when the process value increases. Reverse operati...