Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 601 - 62026275
FAQ00759 for Level Switches | OMRON Industrial Aut...

... the 61F-GP-N. The voltage and current between the 61F electrodes is only about 8 VAC and 1 mA, so it is best to use a float switch contact that is for a minimal load. 61F-G[]N Improved Desig...

https://www.ia.omron.com/support/faq/answer/33/faq00759/

FAQ00844 for Level Switches | OMRON Industrial Aut...

... cable and power cable in the same duct? Answer  There is a possibility of improper operation, so avoid wiring the cables in the same duct or close together. Since there is a weak current (a...

https://www.ia.omron.com/support/faq/answer/33/faq00844/

FAQ00853 for Level Switches | OMRON Industrial Aut...

...e is no problem. In some cases, however, the tank has insulation coating on its internal walls, so make sure to check in advance that the system operates correctly. However, do not use this m...

https://www.ia.omron.com/support/faq/answer/33/faq00853/

faq03253

... However, when there are waves on the liquid surface, 61F will also repeatedly turn ON and OFF, so the lifetime of the contacts will be shorter than usual. 61F-G Example Applicable Models 61F...

https://www.ia.omron.com/support/faq/answer/33/faq03253/

FAQ00948 for Rotary Encoders | OMRON Industrial Au...

... 0, but from an intermediate code, and thus when actually using a code it must first be shifted so that it starts from 0. The example in the code table shows 36 divisions. For the change from...

https://www.ia.omron.com/support/faq/answer/34/faq00948/

FAQ00978 for Rotary Encoders | OMRON Industrial Au...

...[]H 3. Please confirm ON point of phase "Z" output on the controller side and adjust the origin so cut face "D" and phase "Z" origin of other models are not suitable. E2E Standard Sensors for...

https://www.ia.omron.com/support/faq/answer/34/faq00978/

FAQ01209 for Pressure Sensors | OMRON Industrial A...

... Pressure Sensor is ±5% FS. Converting this into voltage, ±5% × 1⁄1000 (%) × 4 V (FS) = ±0.2 V, so the line will deviate ±0.2 V max. E2E Standard Sensors for Detecting Ferrous Metals under St...

https://www.ia.omron.com/support/faq/answer/35/faq01209/

FAQ01327 for Pressure Sensors | OMRON Industrial A...

...7.5006 x 10 -3 0.10197 1 Examples: How many kgf/cm 2 is 10 Pa? Pa = 1.0197 x 10 -5 (kgf/cm 2 ), so 10 Pa = 10 -4 (kgf/cm 2 ). How many Pa is 10 kgf/cm 2 ? 1 kgf/cm 2 = 0.0980665 Mpa, ...

https://www.ia.omron.com/support/faq/answer/35/faq01327/

FAQ02207 for General Purpose Relays | OMRON Indust...

... measure the voltage on both sides of the Relay coil terminal, and set the power supply voltage so that the rated voltage is applied. If wiring is performed over a long distance in parallel w...

https://www.ia.omron.com/support/faq/answer/36/faq02207/

faq02758

...con, Sulfuric, or Organic Gas) Do not use Relays in a location where silicon gas, sulfuric gas (SO 2 or H 2 S), or organic gas is present. If Relays are stored or used for an extended period ...

https://www.ia.omron.com/support/faq/answer/36/faq02758/

faq02761

... 3 km.) Example: For MY4 Relays 100 VAC, 60 Hz, MY4 with CW Cable Answer: Value exceeds 3,000 m so there is no problem with cables up to 3 km. MY Best-selling, general-purpose relays that can...

https://www.ia.omron.com/support/faq/answer/36/faq02761/

FAQ02783 for General Purpose Relays | OMRON Indust...

...ks to their contact form. However, this theory is not applied for high power load applications, so that a single contact point without AU plating is adopted. Contact reliability in minimum lo...

https://www.ia.omron.com/support/faq/answer/36/faq02783/

faq02795

...pose Relays can be mounted? Answer  There are no restrictions. However, it is best to mount MY so that vibration and shock will not be applied in the direction of movement of the contacts. A...

https://www.ia.omron.com/support/faq/answer/36/faq02795/

FAQ02800 for General Purpose Relays | OMRON Indust...

...General Purpose Relays' lifetime? Answer  Welding, contact failure, insulation degradation and so on are cited as the measures used to judge the General Relay's lifetime. Measures used to ju...

https://www.ia.omron.com/support/faq/answer/36/faq02800/

faq02803

...s replaced with MY2N-D2? Answer  Yes, the same Sockets can be used. MY2N-D2 has coil polarity, so take care when wiring. MY Best-selling, general-purpose relays that can be selected based on...

https://www.ia.omron.com/support/faq/answer/36/faq02803/

faq02828

...gainst Leakage Current when Using Proximity Sensors and Relays Connect the bleeder resistor and so that the leakage current that normally flows through the load (Relays coil) is by-passed. AC...

https://www.ia.omron.com/support/faq/answer/36/faq02828/

faq03198

...upported by G7J, it can be used. 4.G7J Relays with AC coils have built-in full-wave rectifiers, so the rated current will be reduced by half or even a third. For this reason, if Solid-state R...

https://www.ia.omron.com/support/faq/answer/36/faq03198/

FAQ01846 for Push Buttons / Indicator Lamps | OMRO...

... the lighting part? Answer  The following models are not provided with a limiting resistor and so it is necessary to connect an external resistor. Pushbutton Switches "A3D", "M2D", "A3A" The...

https://www.ia.omron.com/support/faq/answer/38/faq01846/

FAQ01922 for Push Buttons / Indicator Lamps | OMRO...

...s compatible with the applied voltage? 3. Terminals of the LED and the switch are separated and so it is necessary to connect them. The terminal layout of the A16 is as follows. 61F-G[]N Impr...

https://www.ia.omron.com/support/faq/answer/38/faq01922/

faq00314

...ting temperature range. Generally, the sensing distance will increase at high temperatures, and so the operating point and reset point will both increase, the differential (i.e., the differen...

https://www.ia.omron.com/support/faq/answer/41/faq00314/

結果 601 - 62026275

国/地域選択

Related Contents