Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 9761 - 978061827
PDFSYSMAC CX-Protocol 1.9版 CXONE-AL@@C-V4/AL@@D-V4

...双引号之间指定,例如“12345”。 “12345” 十六进制数据在中括号中指定,例如[5A2B]。 [5A2B] 控制代码通过从列表中选择特殊代码(例如CR、LF或 STX)来指定。 为CR指定[OD] 93 通信报文属性第3-4章 Y...

https://www.fa.omron.com.cn/data_pdf/mnu/w344-cn5-12_cx-protocol.pdf

PDFCX-Simulator Ver. 2.0 CXONE-AL@@D-V4

...acter is included for the TXD instruction, it will be dis- played in a hexadecimal value. (e.g. CR+LF as <0D><0A) •Copy to clipboard The contents of the display buffer in the Message Display ...

https://www.fa.omron.com.cn/data_pdf/mnu/w366-e1-16_cx-simulator.pdf

PDFCJ1W-TC@@@ 温度控制单元 操作手册 2003年3月

...又合上时,电阻限制流到负载的电流。 电容器的介电强度必须是200~300 V。 如果是交流回路,应使用无极性的电容器。 CRᮍ⊩ᛳᗻ䋳䕑电源 C R xix 符合EC导则6 当切换象白帜灯那样具有高涌入电流的负载时,用下...

https://www.fa.omron.com.cn/data_pdf/mnu/w396-c1-01_cj1w-tc.pdf

PDFOPERATION MANUAL Cat. No. W396-E1-03

...pened and the moment the load is reset, caused by this method is longer than that caused by the CR method. The reversed dielectric strength value of the diode must be at least 10 times as lar...

https://www.fa.omron.com.cn/data_pdf/mnu/w396-e1-03_cj1w_tc.pdf

PDFCat. No. W442-E1-01 SYSMAC REFERENCE MANUAL

...&1. End code usage EndExist INT &0 &0 to &2 &0: None (Receive data size specified.) &1: Use &2: CR+LF End code EndCode INT &0 0x0000 to 0x0OFF Note: Valid only when End code usage is set to &...

https://www.fa.omron.com.cn/data_pdf/mnu/w442-e1-01_fb_library.pdf

PDFOPERATION MANUAL Cat. No. W452-E1-08

...pened and the moment the load is reset, caused by this method is longer than that caused by the CR method. The reversed dielectric strength value of the diode must be at least 10 times as lar...

https://www.fa.omron.com.cn/data_pdf/mnu/w452-e1-08_nsj_setup.pdf

PDFMachine Automation Controller NX-series

...particularly lamps with filaments). •If noise causes malfunctions, use countermeasures, such as CR surge absorbers and diodes, for noise sources of input devices and output load devices, as r...

https://www.fa.omron.com.cn/data_pdf/mnu/w519-e1-18_nx-ecc20_.pdf

PDFMachine Automation Controller NX-series

...cuit examples are listed in the following table. Circuit Current Feature Required element AC DC CR meth- od ¡¡If the load is a relay or sol- enoid, there is a delay in the resetting time. If ...

https://www.fa.omron.com.cn/data_pdf/mnu/w521-e1-13_nx-id_ia_oc_od_md.pdf

PDFMachine Automation Controller NJ-series

...MMUNI- CATING None Communications are established. (10) --- Any entry to NOT COMMUNICATING WAIT CR FROM HOST None Wait for Establish Communications Request (S1,F13) from host. (14) COMMUNI- C...

https://www.fa.omron.com.cn/data_pdf/mnu/w528-e1-06_nj501-1340.pdf

PDFMachine Automation Controller NX-series

...particularly lamps with filaments). •If noise causes malfunctions, use countermeasures, such as CR surge absorbers and diodes, for noise sources of input devices and output load devices, as r...

https://www.fa.omron.com.cn/data_pdf/mnu/w536-e1-11_nx-eic202.pdf

PDFIndustrial PC Platform NY-series

...ir wires for pilot lamps (and particularly lamps with filaments). •Use countermeasures, such as CR surge absorbers and diodes, for input device and output load device noise sources, as requir...

https://www.fa.omron.com.cn/data_pdf/mnu/w553-e2-16_nyb.pdf

PDFIndustrial PC Platform NY-series

...ir wires for pilot lamps (and particularly lamps with filaments). •Use countermeasures, such as CR surge absorbers and diodes, for input device and output load device noise sources, as requir...

https://www.fa.omron.com.cn/data_pdf/mnu/w555-e2-16_nyp.pdf

PDFMachine Automation Controller NX-series

...ir wires for pilot lamps (and particularly lamps with filaments). •Use countermeasures, such as CR surge absorbers and diodes, for input device and output load device noise sources, as requir...

https://www.fa.omron.com.cn/data_pdf/mnu/w578-e1-15_nx1p2.pdf

PDFIndustrial PC Platform NY-series

...ir wires for pilot lamps (and particularly lamps with filaments). •Use countermeasures, such as CR surge absorbers and diodes, for input device and output load device noise sources, as requir...

https://www.fa.omron.com.cn/data_pdf/mnu/w580-e2-06_ny512-a6001xx21391x.pdf

PDFMachine Automation Controller NX-series

...ir wires for pilot lamps (and particularly lamps with filaments). •Use countermeasures, such as CR surge absorbers and diodes, for input device and output load device noise sources, as requir...

https://www.fa.omron.com.cn/data_pdf/mnu/w593-e1-15_nx102.pdf

PDF操作手册 Cat. No. W613-CN5-02 SYSMAC CP系列

...、二极管等元件。 ·当切换为浪涌电流较高的负载(如白炽灯)时,应按下图所示抑制浪涌电流。 电路电流特性要素 AC DC CR法 OK OK 如果负载为继电器或螺线管,则在电路断开瞬间和负载重新接入瞬间会出现一个延...

https://www.fa.omron.com.cn/data_pdf/mnu/w613-cn5-02.pdf

PDFUSER’S MANUAL Cat. No. W613-E1-03

...ppress the inrush current as shown below. Circuit Current Characteristic Required element AC DC CR method OK OK If the load is a relay or solenoid, there is a time lag between the moment the ...

https://www.fa.omron.com.cn/data_pdf/mnu/w613-e1-03_cp2e.pdf

PDFUSER’S MANUAL Cat. No. W614-E1-03

...F hex 2-3-5 End Code None (Received Bytes) Received Bytes (no end code) When power is turned ON CR, LF Set End Code 2-3-6 Received Bytes (setting) 256 bytes 256 bytes When power is turned ON ...

https://www.fa.omron.com.cn/data_pdf/mnu/w614-e1-03_cp2e.pdf

PDFMachine Automation Controller NX-series

...ir wires for pilot lamps (and particularly lamps with filaments). •Use countermeasures, such as CR surge absorbers and diodes, for input device and output load device noise sources, as requir...

https://www.fa.omron.com.cn/data_pdf/mnu/w629-e1-08_nx502-1_00.pdf

PDFC200HW-MC402-E Motion Control Unit

...ed and will take the numerical value of this string which is terminated with a carriage return <CR...

https://www.fa.omron.com.cn/data_pdf/mnu/w903-e2-2_c200hw-mc402-e.pdf

結果 9761 - 978061827

国/地域選択

Related Contents