| IAグローバル検索 |
...ed from the ID Controller to the host computer are in the following format: X X X X ......... X∗CR 1 frame = 266 characters max. Header Text Terminator Type Description Header Command Two-cha...
https://www.fa.omron.com.cn/data_pdf/mnu/z083-e1-04a_v600-cd1d-v_.pdf
...Stop bits Selects whether one or two stop bits are to be used. D. Delimiter Sets the delimiter. CR: CR only used. LF: LF only used. CR + LF: CR and LF used. F. Flow...
...r be- tween the CPU and a Memory Card. File I/O Delimiters used Version 1.jj Version 2.00 Input CR+LF or LF CR+LF or CR Output CR+LF CR+LF As shown in the ...
...ss 0000H to 0001H are read. Use one of the following commands to check the battery status. (The CR at the end of each command means carriage return.) a) Read command: RD H/A 1 0000 02*...
https://www.fa.omron.com.cn/data_pdf/mnu/z127-e1-04_v600-h07_h11_d_k___.pdf
...th the data 12345678. POWER OPERATING ALARMS BUSY ERROR SOH Node No. Command code Test data FCS CR Data 1 Data 2 Data 3 Data 4 01h011012345678080Dh SOH Node No. Response code Test data F...
https://www.fa.omron.com.cn/data_pdf/mnu/z167-e1-06a_v640-ham11-v2_hs61_v700-l22_11.pdf
...00,000. Start address number specification range (@@@0H to @@@5H or @@@8H to @@@DH) FCS M××D75 *CR @ Unit No. End code 75: Within specified number of overwrites 76: Exceeded specified number ...
https://www.fa.omron.com.cn/data_pdf/mnu/z194-e1-03_v600-idsc02_04.pdf
... MON - - MEAS CLEAR - - VERSION - - THROUGH - - FREEZE - - MODE COMPOWAY,NORMAL COMPOWAY DELMIT CR, LF, CR+LF CR BLACK, WHITE WHITE COLOR DIRECTION SENSITIVE, NORMAL, ROUGH ...
...NON NON, ODD, EVEN STOP 1BIT 1BIT, 2BIT BAUDRAT 38400 9600, 19200, 38400, 57600, 115200 DELIMIT CR CR, LF, CR+LF COM MODE COMPWAY COMPWAY, NORMAL p.4-12 NODE 0 0~16 KEYLOCK...
https://www.fa.omron.com.cn/data_pdf/mnu/z208-cn5-01_zs-l.pdf
...NON NON, ODD, EVEN STOP 1BIT 1BIT, 2BIT BAUDRAT 38400 9600, 19200, 38400, 57600, 115200 DELIMIT CR CR, LF, CR+LF COM MODE COMPWAY COMPWAY, NORMAL p.4-12 NODE 0 0 to 16 KEYLO...
https://www.fa.omron.com.cn/data_pdf/mnu/z208-e1-04_zs-l.pdf
...th the data 12345678. POWER OPERATING ALARMS BUSY ERROR SOH Node No. Command code Test data FCS CR Data 1 Data 2 Data 3 Data 4 01h011012345678080Dh SOH Node No. Response code Test data F...
https://www.fa.omron.com.cn/data_pdf/mnu/z218-e1-01a_v640-ham12_hs62.pdf
... 1 bit* or 2 bits Header/Footer Prefix None*, 02
https://www.fa.omron.com.cn/data_pdf/mnu/z222-e1-01_v400-h101_201.pdf
...p Bit 1sbit * or 2 bits Header/Footer Prefix None*, 02
https://www.fa.omron.com.cn/data_pdf/mnu/z228-e1-03_v400-h111_h211.pdf
...Up to two Extension Cables can be daisy-chained.) - Extension cable for a long distance ZS-XC_ _CR: within 27m (including Sensor Head. Digital equalizer ZS-XEQ and the Digital equalizer conne...
https://www.fa.omron.com.cn/data_pdf/mnu/z236-e1-08_zs-hl.pdf
...62 characters max. Host Device Response Test data in response Command Command code TS MRON 2 2 *CR Terminator 14 FCS 0 2 @ 3 Controller No. 2 O 5 Test data Response Command code TS MRON 2 2 *...
https://www.fa.omron.com.cn/data_pdf/mnu/z239-e1-04_v600-ca5d0_.pdf
...T OFF, ODD, EVEN OFF 1, 2 1 BAUDRATE 9600, 19200, 38400, 57600, 115200 38400 NODE 0̚16 0 DELMIT CR, LF, CR+LF CR 䆒ᅮ䗝ᢽ/䆒ᅮ㣗ೈ咬䅸ؐ义ⷕ ˄*8˅ҙᔧᬒ఼ऩܗЎ㒘ড়ᅝ㺙ᯊᠡᰒ⼎ℸ㦰ऩDŽ LOCK MOD...
https://www.fa.omron.com.cn/data_pdf/mnu/z240-cn5-03_zfv-c.pdf
...FF, ODD, EVEN OFF 1, 2 1 BAUDRATE 9600, 19200, 38400, 57600, 115200 38400 NODE 0 to 16 0 DELMIT CR, LF, CR+LF CR Settings Selection/Setting Range Default Page LOCK MODE SWIT...
https://www.fa.omron.com.cn/data_pdf/mnu/z240-e1-05_zfv-c.pdf
...inning (header) of the command format. No symbol will be selected if [None] is selected. Suffix CR*/CR+LF/ETX/LF Select the symbol that indicates the end (footer) of the command form...
https://www.fa.omron.com.cn/data_pdf/mnu/z242-e1-04_v400-f050_f250_f350.pdf
...ccessfully or the setting was NG: The delimiter can be selected from the following three types: CR/LF/CR+LF MEASURE -30CR ZFV-CA10 1.000CR Version OKCR ERCR 1feature.fm 3ページ200...
https://www.fa.omron.com.cn/data_pdf/mnu/z244-e1-01_zfv-c.pdf
...B port. Antenna RF Tag Distance level 1 2 3 4 5 6 16 Bar indicator Monitor display DL 06 1 0 * [CR] Antenna channel ("1": channel 1, "2": channel 2) Distance level ("01" to "06") Resend Flag ...
https://www.fa.omron.com.cn/data_pdf/mnu/z249-e1-12_v680-ca5d0_-v2.pdf
...he measurement image and model image are output as a correlation value. (0 to 100) Correlation (CR) Measurement position The X, Y coordinates of the position where the model was found are out...
https://www.fa.omron.com.cn/data_pdf/mnu/z251-e1-04_zfx-c10.pdf