| IAグローバル検索 |
...on] - [Data].) Communication speed USB2.0-compliant Data length - Parity - Stop bit - Delimiter CR, LF, CR+LF Transmission protocol Normal (Note, however, that XMODEM protocol is use...
https://www.fa.omron.com.cn/data_pdf/mnu/z252-e1-03_zfx-c10.pdf
...data retention, writes the same data to all of the tag memory in use. Command : RDSTH100100006*[CR] Reseponse : RD0010001122334455*[CR] Command : WTSTH10010001122334455*[CR]...
https://www.fa.omron.com.cn/data_pdf/mnu/z262-e1-10_v680.pdf
..., ODD (odd), EVEN (even) (default value: NONE) HD.FT (header/footer selection) ST.ET (STX+ETX), CR, CR.LF (CR+LF) (default value: CR) Select [SPCL]. Select [IFU] or...
https://www.fa.omron.com.cn/data_pdf/mnu/z263-e1-05_zx-gt.pdf
...he measurement image and model image are output as a correlation value. (0 to 100) Correlation (CR) Measurement position The X, Y coordinates of the position where the model was found are out...
https://www.fa.omron.com.cn/data_pdf/mnu/z264-e1-09_zfx-c.pdf
...on] - [Data].) Communication speed USB2.0-compliant Data length - Parity - Stop bit - Delimiter CR, LF, CR+LF Transmission protocol Normal (Note, however, that XMODEM protocol is use...
https://www.fa.omron.com.cn/data_pdf/mnu/z265-e1-06a_zfx-c.pdf
...10 0011 0012 0013 0014 “O” “M” “R” “O” “N” 4 5 4 4 4 D 2 F F E 1 byte •RF Tag WT 10 A00 RO OM 1 CR N WT 10 A00 RO OM 1 CR N ST Command code Start address Write data ASCII setting Pro...
https://www.fa.omron.com.cn/data_pdf/mnu/z272-e1-09_v680-chud_ch1d.pdf
...N ( 8 H X h x 9 HT EM ) 9 I Y i y A LF SUB * : J Z j z B VT ESC + ; K [ k { C FF FS , < L¥l | D CR...
https://www.fa.omron.com.cn/data_pdf/mnu/z280-e1-09_g3pw.pdf
...ON, ODD, EVEN STOP BIT 1BIT 1BIT, 2BIT BAUD RATE 38400 9600A19200A38400A57600 A115200 DELIMITER CR+LF CR, LF, CR+LF PASSWORD ON/OFF OFF p.3-20 CHANGE (SET) (Displayed only w...
...ctric sensor, etc. Sensor Head-Controller extension cable (option) Extension cable (*1) ZG2-XC__CR: (3 m, 8 m, 15 m, 25 m) (flexible cable) Cable for Sensor: 0.5 m, 2 m (flexible cable) Exclu...
... (default value: 1BIT) BAUDRAT 9600, 19200, 38400, 57600, 115200 (default value: 38400) DELIMIT CR, LF, CR+LF (default value: CR) NODE 0 to 16 (default value: 0) This "node ...
https://www.fa.omron.com.cn/data_pdf/mnu/z289-e1-03_zg2-dsu.pdf
... Node No.1 is tested with the data 12345678. •1:1 Protocol •1:N Protocol Command code Test data CR Data 1 Data 2 Data 3 Data 4 10123456780Dh Response code Test data CR Data 1 Data 2 ...
https://www.fa.omron.com.cn/data_pdf/mnu/z307-e1-02_v640-ham11-v3.pdf
... 81. A test is preformed for the Amplifier Unit using the data 12345678. Command code Test data CR Data 1 Data 2 Data 3 Data 4 10123456780Dh Response code Test data CR Data 1 Data 2 ...
https://www.fa.omron.com.cn/data_pdf/mnu/z308-e1-02_v640-ham11-etn.pdf
...t registered error, −15: Out of range error C Count This is the number of models found. 0 to 32 CR[0] to CR[31] Correlation This is the correlation of the Nth model that was found. 0...
https://www.fa.omron.com.cn/data_pdf/mnu/z314-e1-05_fq-ms12.pdf
...Y This is the Y coordinate of the position where the model was found. 99999.9999 to 99999.9999 CR Correlation This value indicates how similar the image is to the image registered as referen...
https://www.fa.omron.com.cn/data_pdf/mnu/z315-e1-01_fq-cr1.pdf
...Y This is the Y coordinate of the position where the model was found. −99999.9999 to 99999.9999 CR Correlation This value indicates how similar the image is to the image registered as referen...
https://www.fa.omron.com.cn/data_pdf/mnu/z329-e1-02_fq-cr1_____-m.pdf
... setting) Stop bit 1 bit (Factory default setting) Header None (Factory default setting) Footer CR (Factory default setting) Reading valid time Trigger + 2 sec. (Factory default setting) Proc...
https://www.fa.omron.com.cn/data_pdf/mnu/z333-e1-04_v400-r2.pdf
...op Bit 1sbit* or 2 bits Header/Footer Prefix None*, 02
https://www.fa.omron.com.cn/data_pdf/mnu/z334-e1-03_v500-r2.pdf
...sults of position compensation processing. Applying the Results of Position Compensation: p.104 CR Correlation This is the correlation. 0 to 100 Parameter Setting Description Judgement -2: No...
https://www.fa.omron.com.cn/data_pdf/mnu/z337-e1-12_fq2-s_ch.pdf
...put. •Code Conversion The converted codes are outputted for the following character codes. Note CR Before conversion After conversion LF &h0D &h7F &h8541 DEL &h8543 Character code &h0A &hFF &...
https://www.fa.omron.com.cn/data_pdf/mnu/z338-e1-05_fq2-s_ch.pdf
...统用户手册第3章通信准备工作 ■未使用SECS时使用数据12345678测试1号节点。 •1:1协议 •1:N协议命令代码测试数据 CR 数据1数据2数据3数据4 10123456780Dh 响应代码测试数据 CR 数据1数据2数据3数据...