| IAグローバル検索 |
...W) ● E3JM E3NC-L Not Applicable E3NC-S E3RA E3RB E3S-C E3S-CL E3S-DB E3S-DC E3S-LS3[] E3S-R E3T E3Z/E3Z-[]-UL E3Z-[]-IL[]/E3Z-[]-IL[]-UL E3Z-F E3Z...
...lass 1 (Laser Notice No.56) E3AS-HL 1920014 E3AS-F 1920014 E3C-L[][][]N Series 0222665 Class II E3Z-LR/LT/LL E3Z-LR[][]-UL/LT[][]-UL/LL[][]-UL 1010248 Class 1 (Laser Notice No.56) E3...
...Series changes the “way of using” reflective photoelectric sensors IO-Link Photoelectric Sensor E3Z-[]-IL[] IO-Link Makes Sensor Level Information Visible and Solves the Three Major Issues at...
...by the background. BGS (Background Suppression) and FGS (Foreground Suppression) When using the E3Z-LS61, E3Z-LS66, E3Z-LS81, or E3Z-LS86, select the BGS or FGS fun...
...って入力し、「検索」ボタンをクリックしてください。入力したキーワードを含む検索結果を表示します。 (例)センサ 透過形 E3Z ※アルファベットの大文字と小文字の区別はありません。半角カタカナもご...
...Supplies How to access to the Model Number information For example, on the Photoelectric Sensor E3Z page, you can go to the new “Item Index” tab, and easily select the desired Model Number....
...er processing for customers. An example can be found here: http://www.ia.omron.com/product/item/e3z_1025e/index.html As of March 2008, specifications for approximately 4,000 globally-availab...
...to move to a page with detailed information about that product. [Note] "Catalogue" : e.g., E2E, E3Z "Item" : e.g., E2E-C1B1 2M, E3Z-D61 2M 2.Display of the Number of Hits and Product...
...ors with Separate Digital Amplifiers E3C-LDA Laser Photoelectric Sensor with Built-in Amplifier E3Z-LT / LR / LL Transparent Object Detection Sensor E3S-R UV Power Monitor F3UV Applications P...
...End-User: Ivers-Lee Solution Full ILO+S solution. NX1 controller, 1S servo drive, MX2 inverter, E3Z laser sensors, V430 barcode readers, SL safety curtains, S8VK power supply Value Added Flex...
https://www.omron-ap.co.in/solution/robotics-and-vision-solutions
...ject is further than a setting distance when the amount of receiving light is N
...-RS3. This does not apply, however, to Photoelectric Sensors for detecting transparent objects (E3Z-B, E3S-R, E3S-CR62/67, E32-R21, and E32-R16) or to the E3T. Explanation: The following tabl...
...d time. Immersion to a depth of 1 m for 30 min. Typical models that provide IP67 protection are E3Z Series Photoelectric Sensors, E3S-A/B Series, and E32 Series. For details, refer to Sensors...
...l interference prevention filters are as follows. E39-E6 for E3S-A E39-E8 for E3S-B E39-E11 for E3Z-T[][]A 4. Mutual interference prevention by adjusting sensitivity When sensing distance is ...
... the receiver, which enables a longer sensing distance. For reference, the sensing distance for E3Z-R Photoelectric Sensors are 3 m with the E39-R1 and 4 m with the E39-R1S. E2E Standard Sens...
...by ski goggles. The sensing distance with E39-R1K is the same as with E39-R1. For example, with E3Z-R Photoelectric Sensors with built-in amplifier, the sensing distance is 3 m whether E39-R1...
...C E3S-CL E3S-DB E3S-DC E3S-GS3[]4 E3S-LS3[] E3S-R E3T E3T-[]-UL E3X-HD E3X-SD / NA E3X-ZV / MZV E3Z E3Z-G E3Z-LS E3Z-LT / LR / LL E3Z-[]-IL[] E3Z-...
...L E3S-DB E3S-DC E3S-GS3[]4 E3S-LS3[] E3S-R E3T E3T-[]-UL E3X-HD E3X-SD / NA E3X-ZD E3X-ZV / MZV E3Z E3Z-G E3Z-LS E3Z-LT / LR / LL E3Z-[]-IL[] E3Z-...
...列 K8 系列 F03-16PE 系列 光纖感測器 E3NX 系列 E32 系列 E3X 系列 光電感測器 E39-L / -S / -R 系列 E3JK 系列 E3JM 系列 E3Z 系列 E3T 系列 E3S 系列 近接感測器 E2S 系列 E2E 系列 E2EC 系列 E2F 系列...
...上。 *3. 設置時,感測器需與背景保持120mm以上。 更新日期 2015年8月8日 感測器 光電感測器 放大器內建型 E3AS系列 E3Z-[]-IL[] E3S-DC E3S-DB E3FA, E3RA, E3FB, E3RB E3T E3Z E3ZM-V E3ZM-C E...