Question
Can the EE-SX671 Photomicro Sensor be used in a magnetic field?
Answer
Yes, it is fundamentally possible to use EE-SX671 in a DC magnetic field, but operation must be confirmed by testing if the magnetic field is strong (on the level of affecting electronic circuits) or if EE-SX671 is used near the source of a high-frequency magnetic field.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions