Page top

Lead Contents

FAQ00069 of Programmable Controllers FAQ

FAQ No. FAQ00069

Primary Contents

Question

Can NT-AL001-E RS-232C/RS-422 Link Adapter be used to convert the peripheral port on a CPU Unit of Programmable Controllers to RS-422?

Answer



No, the peripheral port on the CPU Unit of Programmable Controllers do not supply 5 V, so the NT-AL001-E cannot be connected. Use an RS-232C port.