Question
Using CX-Programmer FA Integrated Tool Package, how can we connect Programmable Controller via Ethernet?
Answer
1. Personal Computer Ethernet setting by IP Address and Subnet Mask.
2. Ethernet Unit: IP Address, Node No., Unit No.
3. CX-Programmer and CS1 Programmable Controller is connected with Tool bus Cable.
4. CX-Programmer I/O table Window: Unit Setting (CPU bus unit System Setting) is required to be set for Ethernet [IP Address Conversion] by Automatic generation, [Sub net mask] is set.
5. CX-Programmer (CX-Net): FINS Local Routing table is created and transferred to CS1.
6. Personal Computer issues PING Command to check if Ethernet connection is OK.
7. CX-Programmer Communication Setting
1) Personal Computer Model Change / [Network Type] is set [Ethernet].
        2) Click [Setting], set FINS destination address [Network] / [Node] 
(Node = Ethernet Unit Node Number, Network = Network address set in Routing table)
3) Check Automatic generation method at [Driver] tab / Workstation node Address. Port Number = 9600.
 What products are recommended as substitutes for the C200H-CPU01 Programmable Controller?
What products are recommended as substitutes for the C200H-CPU01 Programmable Controller?
                 How can I connect a C200H Programmable Controller's CPU Unit with an IBM PC/AT or compatible computer?
How can I connect a C200H Programmable Controller's CPU Unit with an IBM PC/AT or compatible computer?
                 Why communication error occurs during CX-Programmer FA Integrated Tool Package get online with Programmable Controller?
Why communication error occurs during CX-Programmer FA Integrated Tool Package get online with Programmable Controller?