Page top

Lead Contents

FAQ00439 of Programmable Controllers FAQ

FAQ No. FAQ00439

Primary Contents

Question

What is the difference between CPM2C Programmable Controllers CPU Units with sinking outputs and sourcing outputs?

Answer



With sinking outputs, current flows in the following order:
"Positive power supply line" to "Load" to "CPM2C" to "Negative power supply line". This is the same as for an NPN transistor.

With sourcing outputs, current flows in the following order:
"Positive power supply line" to "CPM2C" to "Load" to "Negative power supply line". This is the same as a PNP transistor.

The device being output to will determine whether a sinking or sourcing output should be used.