Page top

Lead Contents

FAQ00512 of Programmable Controllers FAQ

FAQ No. FAQ00512

Primary Contents


Can a C200H-NC111/112/211 Position Control Units be used in a CS1-series Programmable Controllers? Are there any restrictions?


Yes, the C200H-NC111/112/211 can be used in CS1-series Programmable Controllers.

The NC112 and NC111 are allocated 10 words, and the NC211 is allocated 20 words. The unit number range for the NC112 and NC111 is 0 to 9. The unit number range for the NC211 is 0 to 8.