Page top

Lead Contents

FAQ00535 of Programmable Controllers FAQ

FAQ No. FAQ00535

Primary Contents


Is there a cable available that will connect the built-in RS-232C port of CS-series Programmable Controllers CPU Unit to NT-AL001 Option of Programmable Controllers?


Yes, XW2Z-070T-1 (70 cm) and XW2Z-200T-1 (2 m) Cables.

These cables can also be used to connect the C200HX/HG/HE or CQM1H Programmable Controllers to the NT-AL001 RS-232C/RS-422A Link Adapter.