Question
Which OMRON products (general-purpose communications components) can the CPM2C-CIF21 Simplified Communications Unit communicate with?
Answer
CPM2C-CIF21 can perform simplified communications if the connected device is an OMRON Temperature Controllers, Digital Panel Indicators, or Timers.
Communications with general-purpose devices is done using SYSWAY or CompoWay/F commands using a command/response method. Therefore, a connection cannot be established when information flows one-way from the connected device, such as with barcode readers.
Only the following models can be connected:
Temperature Controllers
E5GN, E5CN, E5EN, E5AN, E5CK, E5EK, E5AK, E5EJ, E5AJ, E5AF, and E5ZN
Digital Panel Indicators
K3GN, K3NX, K3NV, K3NR, K3NP, K3NC, K3NH, and K3TS
Timers
H8GN
 What products are recommended as substitutes for the C200H-CPU01 Programmable Controller?
What products are recommended as substitutes for the C200H-CPU01 Programmable Controller?
                 How can I connect a C200H Programmable Controller's CPU Unit with an IBM PC/AT or compatible computer?
How can I connect a C200H Programmable Controller's CPU Unit with an IBM PC/AT or compatible computer?
                 Why communication error occurs during CX-Programmer FA Integrated Tool Package get online with Programmable Controller?
Why communication error occurs during CX-Programmer FA Integrated Tool Package get online with Programmable Controller?