Question
When I send and receive data with protocol macros, occasionally the data header is not received properly. Why?
Answer
If the device that you are connected to using protocol macros has a fast processing time (the time the data is received until the time the data is returned), the protocol macro may not be able to receive all of the data.
When using protocol macros, some time is necessary after sending data from the Programmable Controllers before the Programmable Controllers will be able to receive data.
Refer to the following data; the values are guidelines.
CS1W-SCB21/41-V1 Communications Board, CS1W-SCU21-V1 Communications Unit, or CJ1W-SCU21/41 Communications Unit
| Baud rate (bit/s) | Time lag (μs) | 
| 1200 | 1116 | 
| 2400 | 578 | 
| 4800 | 288 | 
| 9600 | 144 | 
| 19200 | 73 | 
| 38400 | 36 | 
C200HW-COM04-V1 to 06-V1 Communications Board, or CQM1H-SCB41 Communications Board
| Baud rate (bit/s) | Time lag (ms) | 
| 1200 | 30 | 
| 2400 | 15 | 
| 4800 | 8 | 
| 9600 | 5 | 
| 19200 | 3 | 
 What products are recommended as substitutes for the C200H-CPU01 Programmable Controller?
What products are recommended as substitutes for the C200H-CPU01 Programmable Controller?
                 How can I connect a C200H Programmable Controller's CPU Unit with an IBM PC/AT or compatible computer?
How can I connect a C200H Programmable Controller's CPU Unit with an IBM PC/AT or compatible computer?
                 Why communication error occurs during CX-Programmer FA Integrated Tool Package get online with Programmable Controller?
Why communication error occurs during CX-Programmer FA Integrated Tool Package get online with Programmable Controller?