Page top

Lead Contents

FAQ02970 of Programmable Controllers FAQ

FAQ No. FAQ02970

Primary Contents

Question

Are there any cables available to connect the Programmable Controller (PLC) or the Programmable Terminal (PT) to a personal computer's USB port?

Answer



Yes. Use the D-sub to USB-serial conversion cable.

This cable can connect the Programmable Controller "SYSMAC", Programmable Terminal "NT/NS Series", or Programmable Relay "ZEN" to a personal computer's USB port.

Model Number

CS1W-CIF31

Compatible Software Applications

Software applications using the CX-Server or Fins Gateway to communicate with the Programmable Controller

The following software applications are also compatible.

CX-Programmer, CX-Simulator, CX-Protocol, CX-Motion

CX-Position, CX-Process, DeviceNet Configuration Tool

DAIKANYAMA 32, NS-Designer, Windows Version of NT Support Tool (NTST)

*There are Communications (COM) port limitations with the NT Support Tool.

ZEN Support Software (Ver.3.0 and later)

The following OMRON Programmable controllers, Programmable Terminals and Programmable Relays which are supported by the compatible software applications

Programmable Controller

CS/CJ Series, C Series (C200HS, C200HE/HG/HX, C200H/C1000H/2000H, CQM1, CPM1, CPM1A, CPM2A, SRM1, CQM1H, SPM2C), CVM1/CV Series

Programmable Terminal

NS Series, NT Series

Programmable Relay

ZEN

Connector specifications

Personal Computer side: USB (A plug connector, male)

Programmable Controller side: RS-232C (D-sub 9-pin, male)

* "Windows" is a registered trademark of Microsoft Corporation.