Page top

Lead Contents

FAQ01701 of Optical Transmitting Components FAQ

FAQ No. FAQ01701

Primary Contents

Question

What is the difference between free run and handshake operation?

Answer



Free Run

"Free Run" means free-flowing transmission and only SD and RD signals are used.

(Free running is often used for communications between personal computers or Programmable Controllers and devices.)

Handshake

Handshaking refers to the control of transmissions between send/receive devices, e.g., stopping/starting communications during data transmission. (Also called "flow control").

For example, if, during data communications using a modem, the data transmission from the modem to the personal computer system is too fast and the system cannot keep up, the personal computer system must notify the modem to temporarily stop data transmission.

In this way the volume of data is adjusted (suppressed) when sending and receiving data between two nodes by reducing the data transmission speed or stopping transmission to suit mainly the receiving side, e.g., when the reception buffer is full or the processing of received data is not finished in time.

Applicable Model: Z3R Optical RS-232C Link Module

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization. Meet the Industry Standard in Fan Ionizers.

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Optical Transmitting Components FAQ