Question
What devices are required for optical transmissions?
Answer
Two Optical Link Modules and one Optical Fiber are required for optical transmissions. An AC Adapter will also be required for Z3R-[][]12 and Z3G Optical Link Modules.
There are two types of Optical Link Module: the Z3R RS-232C and the Z3G GP-IB. (See 1 and 2 in the following diagram.)
Applicable models: Z3R(Optical RS-232C Link Module) Series, Z3G(Optical GP-IB Link Module)
New Models with Indication Monitor and Simple Functions for Easy System Commissioning
High-speed, High cost performance Ionization. Meet the Industry Standard in Fan Ionizers.
Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.