Page top

Lead Contents

FAQ01735 of Optical Transmitting Components FAQ

FAQ No. FAQ01735

Primary Contents

Question

What is an interface?

Answer



The word interface means a "border" and refers to the hardware that governs data transmissions between two or more devices.
The general-purpose interfaces that are commonly used are shown in the following diagram.

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization. Meet the Industry Standard in Fan Ionizers.

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Optical Transmitting Components FAQ