Page top

Lead Contents

FAQ01751 of Optical Transmitting Components FAQ

FAQ No. FAQ01751

Primary Contents

Question

What are RS-422 and RS-485?

Answer



Both are standards set by the EIA in relation to electrical characteristics of balanced interfaces (e.g., drivers and receivers) and there are many similarities between the two standards.

With RS-422, more than one receiver (signal receiver) can be connected to one driver (signal sender) on the same transmission line but no allowances have been made for multiple drivers.

The RS-485 is an extended version of the RS-422, which allows multiple drivers (with 3-state outputs) and multi-drop (party line) configuration.

RS-422 and RS-485 allow faster transmissions than the RS-232C standard (applicable for baud rates of 20 Kbits/s or less).

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization. Meet the Industry Standard in Fan Ionizers.

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Optical Transmitting Components FAQ