- Improving the density and efficiency to optimize the power supply and electronic circuit protectors
Smart Power Supply (240/480 W)
last update: October 6, 2025
- Improving the density and efficiency to optimize the power supply and electronic circuit protectors
*1. Based on our survey.
A Push-in Plus terminal block can greatly reduce the wiring work compared with a screwed terminal block.
*2. Based on our measurement data for both Push-in Plus and screwed terminal blocks.
Switch on and off the supply voltage of each system with the button on the front of the S8AS2. The current value appears in the front display when the supply voltage is on. Use the display of the power supply system to facilitate the field operation.
The digital display on the front of the S8AS2 allows easy monitoring of the voltages, currents, and maximum currents of each system and all systems.
By visualizing the service life, the product can be used more efficiently, minimizing waste and reducing the workload associated with regular inspections and replacements.
A Power Supply, electronic CPs, and terminal blocks have been integrated into one unit, eliminating the need to prepare multiple devices and evaluate their combination.
Electronic circuit protectors with excellent tripping performance can stabilize circuits at power-on or in case of a device error.
CO2 is one of the greenhouse gas (GHG). Using a more efficient DC Power Supply reduces the power consumed within control panel and consequently reduces CO2 emissions.
Natural disasters caused by global warming and climate change have become global social issue, that drives over 150 countries and regions worldwide to take action toward decarbonization.Our goal is to reduce greenhouse gas (GHG) emissions toward by half through new ways of building control panels, that key figure of the manufacturing site.
This Value Design also integrate environment consideration concept that enable earth and user-friendly control panel building.
eCAD library provided for all models greatly reduces design work. Push-In Plus technology requires only a single step, greatly reducing wiring work.
Unified size and side-by-side mounting help delivering more compact control panels with additional functionality.OMRON Push-In Plus technology for easy wire insertion and firm wire holding ability.
OMRON’s Push-In Plus technology is as easy as inserting to an earphone jack. This reduces the load on worker fingers.
Value Design for Panel (Value Design) is the common concept shared across OMRON’s in-panel product specifications to deliver new value to your control panels.This Value Design also integrate environment consideration concept that enable earth and user-friendly control panel building.
last update: October 6, 2025