Primary Contents

Site Search Results

Site Search Product Search
Results 371 - 380 of 1179
faq01077
...s The result of the addition operation shown in Figure1 cannot be expressed with only 8 digits, so an overflow (i.e., a “carry”) occurs. In this case the Carry Flag (CY) will turn ON. Figure2...

https://www.ia.omron.com/support/faq/answer/26/faq01077/

faq01464
...Are there instructions that directly make comparisons (e.g., "equal", "less than", "more than") so that comparison results do not have to be accessed from the status of result flags for compa...

https://www.ia.omron.com/support/faq/answer/26/faq01464/

faq02260
...ogramming: CS1/CJ1-series Programmable Controllers Figure 1 The Problem with the Ladder Program So what is the problem with the ladder program? To get to the point, there is a problem in the ...

https://www.ia.omron.com/support/faq/answer/26/faq02260/

faq02639
...rlier than 2.0 or a CX-Programmer version lower than 4.0, individual tasks cannot be protected, so the entire program must be protected instead. CJ2 Introducing the Flagship CJ2 CPU Units, wi...

https://www.ia.omron.com/support/faq/answer/26/faq02639/

faq02836
... (D100) + 123 (constant) = 246 (D100) Note:The instruction in Figure 1 will execute each cycle. So when you want to perform the operation A + B = C in realtime when the add command bit (CIO 0...

https://www.ia.omron.com/support/faq/answer/26/faq02836/

faq02890
...mation. Also, the Memory Card can be removed even when power is being supplied to the CPU Unit, so data can be exchanged with personal computers or spreadsheet software while the Programmable...

https://www.ia.omron.com/support/faq/answer/26/faq02890/

FAQ00198 for Programmable Terminals | OMRON Indust...
...s Question In the NS-series Programmable Terminals, is there a way to create a group of buttons so that all of the other buttons go OFF when one of the buttons is ON (i.e., only 1 button can ...

https://www.ia.omron.com/support/faq/answer/27/faq00198/

FAQ00230 for Programmable Terminals | OMRON Indust...
...ary Contents Question The NS-series Programmable Terminal is not equipped with an RS-422A port, so how can it communicate beyond the rated distance for RS-232C (15 m)? Answer  Use an NS-AL00...

https://www.ia.omron.com/support/faq/answer/27/faq00230/

FAQ01111 for Programmable Terminals | OMRON Indust...
...ogrammable Terminal's pin allocation is the same as a Programmable Controller's pin allocation, so use the same cable that is used to connect the computer to a Programmable Controller. The fo...

https://www.ia.omron.com/support/faq/answer/27/faq01111/

FAQ02182 for Basic Switches | OMRON Industrial Aut...
...Countermeasures: Switch the load using a relay or a contactor. A protective circuit is required so that loads such as relays, motors, incandescent bulbs, and solenoids can be used properly. C...

https://www.ia.omron.com/support/faq/answer/29/faq02182/

Results 371 - 380 of 1179