Primary Contents

Site Search Results

Site Search Product Search
Results 361 - 370 of 1179
faq00069
...Answer  No, the peripheral port on the CPU Unit of Programmable Controllers do not supply 5 V, so the NT-AL001-E cannot be connected. Use an RS-232C port. CJ2 Introducing the Flagship CJ2 CP...

https://www.ia.omron.com/support/faq/answer/26/faq00069/

faq00077
...e memory areas. However, the device type is set to CQM1 when using the SYSMAC Support Software, so the check for the usable memory areas, which is normally performed when using CPM2C, will no...

https://www.ia.omron.com/support/faq/answer/26/faq00077/

faq00154
...Link Unit? Answer  Yes. The 3G2A5-LK201-EV1 cannot be used together with the SYSMAC LINK Unit, so switch to the C500-LK203. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifun...

https://www.ia.omron.com/support/faq/answer/26/faq00154/

faq00279
... containing the clock data for programming. The words used for click data depends on the model, so refer to the operation manual. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Mul...

https://www.ia.omron.com/support/faq/answer/26/faq00279/

FAQ00287 for Programmable Controllers | OMRON Indu...
...he Programmable Controller's power supply does not go OFF. The battery service life is 5 years, so replace the battery every 5 years to prevent problems such as electrolyte leakage. CJ2 Intro...

https://www.ia.omron.com/support/faq/answer/26/faq00287/

faq00454
... Negative logic (see note) is much more common among Output Units for Programmable Controllers, so we recommend using models with negative logic. Note:C200H Programmable Controllers Output Un...

https://www.ia.omron.com/support/faq/answer/26/faq00454/

faq00923
... CIO 0. 2.The 8 bits extracted in the previous step must be moved to the lower 8 bits of a word so that they can be used in processing in the next program rung. Use the MOVE DIGITS instructio...

https://www.ia.omron.com/support/faq/answer/26/faq00923/

faq00924
...the MOVE DIGITS instruction (MOVD) could have be used, but this time 6 bits have been extracted so the MOVD instruction cannot be used. Instead, the LOGICAL AND instruction (ANDW) will be use...

https://www.ia.omron.com/support/faq/answer/26/faq00924/

faq01011
... No. FAQ01011 Related Contents Primary Contents Question Can I program Programmable Controllers so that all of the outputs in a ladder program step will not turn OFF, even after proceeding to...

https://www.ia.omron.com/support/faq/answer/26/faq01011/

faq01067
...swer  The water level signal (1 to 5 VDC) from the Liquid Level Indicator is an analog signal, so first it must be converted into a digital signal using an Analog Input Unit. The following i...

https://www.ia.omron.com/support/faq/answer/26/faq01067/

Results 361 - 370 of 1179