Primary Contents

Site Search Results

Site Search Product Search
Results 351 - 360 of 1179
faq01877
...one that is one step higher in capacity. The connected load exceeds the Power Supply's ratings, so it is triggering the overload protection function. Select a different Power Supply with suff...

https://www.ia.omron.com/support/faq/answer/22/faq01877/

faq01991
...e expectancy was calculated by high-temperature testing of the aluminum electrolytic capacitor, so these values are guidelines only. With S8VS Series Switch Mode Power Supply, the Maintenance...

https://www.ia.omron.com/support/faq/answer/22/faq01991/

faq01993
...herwise inoperative. Use identical models for Power Supplies A and B. Select the Power Supplies so that either one can supply the required load capacity. When connecting Power Supplies for ba...

https://www.ia.omron.com/support/faq/answer/22/faq01993/

faq02011
...result in an unbalanced load current, possibly causing the rated output current to be exceeded, so the parallel connection is not possible. Use the same length and thickness of load connectio...

https://www.ia.omron.com/support/faq/answer/22/faq02011/

FAQ01127 for Photomicro Sensors | OMRON Industrial...
...g Load Resistance Values Example description and cause: The load resistance value is too small, so the phototransistor cannot pass the circuit current. (Optical current IL ...

https://www.ia.omron.com/support/faq/answer/24/faq01127/

FAQ01133 for Photomicro Sensors | OMRON Industrial...
...turer responsibility for any resulting deterioration or damage. Be careful to design the system so that operation will be performed within these ratings. In actual operation, derating is used...

https://www.ia.omron.com/support/faq/answer/24/faq01133/

FAQ01138 for Photomicro Sensors | OMRON Industrial...
... leakage of the phototransistor when a specified bias voltage is imposed on the phototransistor so that the polarity of the collector is positive and that of the emitter is negative on condit...

https://www.ia.omron.com/support/faq/answer/24/faq01138/

faq02681
...ight). A circuit to fully stabilize the power supply voltage is not built into the Sensors, and so the voltage supplied to the Sensors will fall when the LED is lit due to the cable resistanc...

https://www.ia.omron.com/support/faq/answer/24/faq02681/

faq02687
...the negative terminal will not result in failure or other problems, but the product is designed so that the L terminal is open or connected to the positive terminal, so leave it open...

https://www.ia.omron.com/support/faq/answer/24/faq02687/

faq00060
.../CJ-series Programmable Controllers are OFF. Other CPU Unit models do not have switch settings, so this does not need to be checked. When There Is a Power Supply Failure Check the power suppl...

https://www.ia.omron.com/support/faq/answer/26/faq00060/

Results 351 - 360 of 1179