... 3 km.) Example: For MY4 Relays 100 VAC, 60 Hz, MY4 with CW Cable Answer: Value exceeds 3,000 m so there is no problem with cables up to 3 km. MY Best-selling, general-purpose relays that can...
...ks to their contact form. However, this theory is not applied for high power load applications, so that a single contact point without AU plating is adopted. Contact reliability in minimum lo...
...pose Relays can be mounted? Answer There are no restrictions. However, it is best to mount MY so that vibration and shock will not be applied in the direction of movement of the contacts. A...
...General Purpose Relays' lifetime? Answer Welding, contact failure, insulation degradation and so on are cited as the measures used to judge the General Relay's lifetime. Measures used to ju...
...s replaced with MY2N-D2? Answer Yes, the same Sockets can be used. MY2N-D2 has coil polarity, so take care when wiring. MY Best-selling, general-purpose relays that can be selected based on...
...gainst Leakage Current when Using Proximity Sensors and Relays Connect the bleeder resistor and so that the leakage current that normally flows through the load (Relays coil) is by-passed. AC...
...upported by G7J, it can be used. 4.G7J Relays with AC coils have built-in full-wave rectifiers, so the rated current will be reduced by half or even a third. For this reason, if Solid-state R...
... the lighting part? Answer The following models are not provided with a limiting resistor and so it is necessary to connect an external resistor. Pushbutton Switches "A3D", "M2D", "A3A" The...
...s compatible with the applied voltage? 3. Terminals of the LED and the switch are separated and so it is necessary to connect them. The terminal layout of the A16 is as follows. 61F-G[]N Impr...
...ting temperature range. Generally, the sensing distance will increase at high temperatures, and so the operating point and reset point will both increase, the differential (i.e., the differen...