| Site Search | Product Search | IA Global Search |
...ssary for developing AI detection performance. The system selects the best images for learning, so anyone can build the optimal AI model—no expert knowledge required. This dramatically saves ...
... have a single wavelength. With high-frequency Modulation, the emitted laser beam is controlled so that it contains multiple wavelengths. Diffuse-reflective Model E3NC-LH02 Long-distance and ...
... Reuse of codes • The 3D simulation is very reliable since it is based on the real system cores so you can reuse the whole programming to control the real machine by significantly shortening ...
...placement sensor, the measurement point remains the same at any position in the measuring range so that precise measurements can always be made. Measurement in narrow area and by the wall Whe...
...g position Angle adjustment up to 330° After fastening to the adapter, you can adjust the angle so that the display is easy to see. 180° reverse display The display can rotate 180°. Useful fu...
...ction in processing quality. • The hydraulic pressure system is divided into multiple sections, so finding degraded packing locations takes time. Solution from OMRON You can use a rise in hyd...
...In a machine operation intervention such as removing a crashed product, the machine is stopped, so there is no production. SOLUTION • You can pickup the product safely with Safely-Limited Spe...
...No special safety measures required for Class 1 laser The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...
...cements in as little as 10 seconds*1 using e-jig Using e-jig eliminates the need for adjustment so that anyone can install in the same position. Easily upgrade existing facilities to enable “...
...ts frequency of automatic measurement allows for understanding the degradation trend, which was so far difficult. K7GE proposes a new way of monitoring insulation. Highly reproducible measure...
...arts feeders, roll presses for secondary batteries, assembly machines for digital products, and so on to detect the presence or absence of workpieces. However, many customers are using fiber ...
...nitoring of motors that frequently change speed, which were difficult to identify abnormalities so far. And simplified condition monitoring device parameter configuration process is contribut...
...t and accurate collection of high‐resolution data in chronological order, the amount of data is so large that the data transfer to databases becomes a bottleneck. [NX5] With approximately fou...
...t having to take a robot out of production. The onscreen display includes a virtual robot stick so users can control the robot just as they would control a physical robot. In addition to the ...
...ngle characteristics of ±85° max. Place the sensors away from the pathways of people and robots so that the sensors do not obstruct their movement. Thus remove failure risks such as optical a...
...ror displayed in multiple languages [PATENT PENDING] *1 ZP-L’s display supports four languages, so that on-site workers at local factories can understand its configuration. Error displays hav...
...nutes to seconds Result of Learn • Tools arranged in reading order • ROIs (Regions of Interest) so each code can be read uniquely • ROI sized to accommodate the expected positional uncertaint...
... using the variable resistor on the dielectric strength testing equipment, or apply the voltage so that it crosses the zero point when it rises or falls. Top of page Maintenance Life Expectan...
https://www.ia.omron.com/support/guide/22/further_information.html
...two contacts are not always going to turn ON/OFF at the same time (there may be a slight delay) so one contact will bear the full load momentarily. What are twin-contact relay models suitable...
https://www.ia.omron.com/support/guide/36/further_information.html
...小負載時,將無法破壞接點表面產生的硫化物膜,導致接點接觸不良。此時請改用金接點微小負載開關。 硫化氣體(H 2 S、SO 2 )、氨氣(NH 3 )、硝酸氣體(HNO 3 )、氯化氣體(Cl 2 )等強腐蝕性氣體或高溫...