Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 361 - 38026275
MD Series Autonomous Mobile Robots/Features | OMRO...

...le and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, so we can grow with your business. Grow Your Business − Modify layouts to optimize production A...

https://www.ia.omron.com/products/family/3951/feature.html

HD Series Autonomous Mobile Robots/Features | OMRO...

...le and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, so we can grow with your business. Grow Your Business − Modify layouts to optimize production A...

https://www.ia.omron.com/products/family/3952/feature.html

NX-CT[][][][] NX-series High-speed Counter Unit/Fe...

...alse positive During inline inspection, variations in conveyor speed prevent capturing an image so that it fits into the camera’s field of view, requiring workpieces to pause or slow down. NX...

https://www.ia.omron.com/products/family/3961/feature.html

Y92[] Accessories/Features | OMRON Industrial Auto...

...e Sensor. Sputter Protective Covers (Threaded on Inside of Cover) • The cover uses Fluororesin, so that chips that adhere due to sputtering can be easily removed. Sputter Protective Covers (N...

https://www.ia.omron.com/products/family/484/feature.html

G70D-SOC08 Relay Terminal/Features | OMRON Industr...

... now be connected with a short bar in the G70D-SOC08. • No tools are required to remove Relays, so Relay replacement is easier than ever. • The attached terminal cover prevents shocks. • Equi...

https://www.ia.omron.com/products/family/863/feature.html

CS Series Programmable Controllers/Features | OMRO...

...e active CPU Unit, the standby CPU Unit takes over in an instant (using the hot standby method) so that system operation continues essentially unaffected. Other duplex variations are also pos...

https://www.ia.omron.com/products/family/9/feature.html

Overview of Cam Positioners | OMRON Industrial Aut...

...age Resolver Unlike Encoders, Resolvers are simply structured and have no electronic components so their performance is virtually unaffected by dust or vibration. This makes them highly relia...

https://www.ia.omron.com/support/guide/12/overview.html

Further Information of Basic Switches Technical Gu...

...Sliding Door 1. Note: 1. Do not use the switch with the actuator continuously pressed in. Doing so may accelerate degradation and change the characteristics. 2. Waterproof Z-D55 Switch The ru...

https://www.ia.omron.com/support/guide/29/further_information.html

Further Information of Limit Switches Technical Li...

...positions highly accurately. The plunger must be installed according to the movement of the dog so that an incorrect load will not be imposed on the plunger. Roller plunger Small Medium Large...

https://www.ia.omron.com/support/guide/30/further_information.html

The Correct Fan Must Be Selected to Prevent Failur...

...the total heating value. Generally speaking, the heating value indicates the power consumption, so you can assume that the power consumption equals the heating value. Heating value(W) = In...

https://www.omron-ap.com/solution/panel/article/article_000793.html

Resolution of Hot Spot | OMRON Industrial Automati...

...erature inside the control panel is often an issue. The inside of the control panel is designed so that air circulates well to release as much heat as possible to the outside, but heat may bu...

https://www.omron-ap.com/solution/panel/article/article_000798.html

faq03420

...ways, can it still detect earthquakes? Answer  The D7G-F senses vibration in the X-Y direction so it cannot detect earthquakes if it is mounted directly onto the machine. Mount it on a fixed...

https://www.ia.omron.com/support/faq/answer/48/faq03420/

Safety I/O Unit - Product Category | OMRON Industr...

...ns or safety output functions. There are 1 products of Safety I/O Unit. Safety I/O Unit NX-SI / SO Build a simple and flexible safety system...

https://www.ia.omron.com/products/category/automation-systems/machine-automation-controllers/ethercat-slave-terminals-nx-series/safety-i_o-unit/

E3NC Smart Laser Sensors/Features | OMRON Industri...

... have a single wavelength. With high-frequency Modulation, the emitted laser beam is controlled so that it contains multiple wavelengths. Diffuse-reflective Model E3NC-LH02 Long-distance and ...

https://www.ia.omron.com/products/family/3316/

NJ501-4[][][] NJ-series NJ Robotics CPU Units/Feat...

... Reuse of codes • The 3D simulation is very reliable since it is based on the real system cores so you can reuse the whole programming to control the real machine by significantly shortening ...

https://www.ia.omron.com/products/family/3387/

Frame - Glossary index | OMRON Industrial Automati...

...emperature Controllers Programmable Terminals An object that enables creating areas on a screen so that only part of the screen can be switched to another page. Frames consist of more than on...

https://www.ia.omron.com/support/glossary/meaning/4443.html

explanation_of_terms.html

...sistance connected in parallel to the load in order to increase apparently small load currents, so that the ON/OFF of minute currents functions normally. PDF Download(8992KB) Local Navigation...

https://www.ia.omron.com/support/guide/18/explanation_of_terms.html

explanation_of_terms.html

...: The difference in the operating times appears as a shift from the central value of operation, so the maximum or minimum values divided by 2 and expressed as plus (+) and minus (-) indicatio...

https://www.ia.omron.com/support/guide/19/explanation_of_terms.html

Further Information of Photomicro Sensors | OMRON ...

...r not the Sensor responds with respect to sensing object edge position. (Design the application so that light will be completely interrupted.) ・ Indicates the discrepancy in the edge positio...

https://www.ia.omron.com/support/guide/24/further_information.html

Reduce Work with Terminal Block Support Tool | OMR...

...rminal Blocks, checking the installation space and applicable wires, and marking can be reduced so that you can easily and efficiently select the Terminal Blocks required to wire your devices...

https://www.omron-ap.com/solution/panel/article/article_000795.html

結果 361 - 38026275

国/地域選択

Related Contents