| IAグローバル検索 |
...Answer No, the peripheral port on the CPU Unit of Programmable Controllers do not supply 5 V, so the NT-AL001-E cannot be connected. Use an RS-232C port. CJ2 Introducing the Flagship CJ2 CP...
...e memory areas. However, the device type is set to CQM1 when using the SYSMAC Support Software, so the check for the usable memory areas, which is normally performed when using CPM2C, will no...
...Link Unit? Answer Yes. The 3G2A5-LK201-EV1 cannot be used together with the SYSMAC LINK Unit, so switch to the C500-LK203. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Multifun...
... containing the clock data for programming. The words used for click data depends on the model, so refer to the operation manual. CJ2 Introducing the Flagship CJ2 CPU Units, with Built-in Mul...
...he Programmable Controller's power supply does not go OFF. The battery service life is 5 years, so replace the battery every 5 years to prevent problems such as electrolyte leakage. CJ2 Intro...
... Negative logic (see note) is much more common among Output Units for Programmable Controllers, so we recommend using models with negative logic. Note:C200H Programmable Controllers Output Un...
... CIO 0. 2.The 8 bits extracted in the previous step must be moved to the lower 8 bits of a word so that they can be used in processing in the next program rung. Use the MOVE DIGITS instructio...
...the MOVE DIGITS instruction (MOVD) could have be used, but this time 6 bits have been extracted so the MOVD instruction cannot be used. Instead, the LOGICAL AND instruction (ANDW) will be use...
... No. FAQ01011 Related Contents Primary Contents Question Can I program Programmable Controllers so that all of the outputs in a ladder program step will not turn OFF, even after proceeding to...
...swer The water level signal (1 to 5 VDC) from the Liquid Level Indicator is an analog signal, so first it must be converted into a digital signal using an Analog Input Unit. The following i...
...s The result of the addition operation shown in Figure1 cannot be expressed with only 8 digits, so an overflow (i.e., a “carry”) occurs. In this case the Carry Flag (CY) will turn ON. Figure2...
...Are there instructions that directly make comparisons (e.g., "equal", "less than", "more than") so that comparison results do not have to be accessed from the status of result flags for compa...
...ogramming: CS1/CJ1-series Programmable Controllers Figure 1 The Problem with the Ladder Program So what is the problem with the ladder program? To get to the point, there is a problem in the ...
...rlier than 2.0 or a CX-Programmer version lower than 4.0, individual tasks cannot be protected, so the entire program must be protected instead. CJ2 Introducing the Flagship CJ2 CPU Units, wi...
... (D100) + 123 (constant) = 246 (D100) Note:The instruction in Figure 1 will execute each cycle. So when you want to perform the operation A + B = C in realtime when the add command bit (CIO 0...
...mation. Also, the Memory Card can be removed even when power is being supplied to the CPU Unit, so data can be exchanged with personal computers or spreadsheet software while the Programmable...
...s Question In the NS-series Programmable Terminals, is there a way to create a group of buttons so that all of the other buttons go OFF when one of the buttons is ON (i.e., only 1 button can ...
...ary Contents Question The NS-series Programmable Terminal is not equipped with an RS-422A port, so how can it communicate beyond the rated distance for RS-232C (15 m)? Answer Use an NS-AL00...
...ogrammable Terminal's pin allocation is the same as a Programmable Controller's pin allocation, so use the same cable that is used to connect the computer to a Programmable Controller. The fo...
...Countermeasures: Switch the load using a relay or a contactor. A protective circuit is required so that loads such as relays, motors, incandescent bulbs, and solenoids can be used properly. C...