| IAグローバル検索 |
...eeder resistance? Answer Bleeder resistance is resistance connected in parallel with the load so that the load current appears to increase in order to correctly switch microloads. MY Best-s...
...d ON, but the zero cross function causes the load current to always flow from a point near zero so that inrush current can be suppressed more compared to Solid-state Relays that do not have t...
...measure. Connect a bleeder resistor as in the figure above and set the bleeder resistance value so that the Solid-state Relay input voltage is 0.5 V max. when the Solid-state Relay is OFF. 2....
...to turn ON, but near point A where there is no current flow the ON status cannot be maintained, so the Solid-state Relay turns OFF and then turns ON when the charge current starts to flow at ...
.... The power interruption compensation function saves the internal clock data and settings only, so the output circuit remains OFF. K3HB-X A Process Indicator Ideal for Discriminating and Disp...
...100 10S ON The specifications are a power supply voltage of 100 VAC with a 10 s power ON delay, so the replacement product should be the 100 to 240-VAC or 100 to 125-VDC H3CR-A8E. Note:The te...
...ion for long periods of time (e.g., a month or longer) under high-temperature conditions. Doing so may reduce the life of the Timer due to deterioration of internal parts, such as electrolyti...
...separate motor and clutch connection. STP socket wiring and H2C-F top wiring are irrelevant and so a large change in wiring is required. The mounting method also must change from STP sockets ...
...nt of the external connection is not compatible. H3AM-NS cannot be used with DC power supplies, so see whether H3CR-A8E can be used to create a substitute function. The size of the panel cuto...
... - 100.8 W = 25.2 W To convert the internal loss to calories: By Joule's law, 1 W = 0.24 cal/s, so 25.2 W = 25.2 × 0.24 cal/s = 6.05 cal/s S8VS Multi-Function Indication Monitor for Productio...
...one that is one step higher in capacity. The connected load exceeds the Power Supply's ratings, so it is triggering the overload protection function. Select a different Power Supply with suff...
...e expectancy was calculated by high-temperature testing of the aluminum electrolytic capacitor, so these values are guidelines only. With S8VS Series Switch Mode Power Supply, the Maintenance...
...herwise inoperative. Use identical models for Power Supplies A and B. Select the Power Supplies so that either one can supply the required load capacity. When connecting Power Supplies for ba...
...result in an unbalanced load current, possibly causing the rated output current to be exceeded, so the parallel connection is not possible. Use the same length and thickness of load connectio...
...g Load Resistance Values Example description and cause: The load resistance value is too small, so the phototransistor cannot pass the circuit current. (Optical current IL ...
...turer responsibility for any resulting deterioration or damage. Be careful to design the system so that operation will be performed within these ratings. In actual operation, derating is used...
... leakage of the phototransistor when a specified bias voltage is imposed on the phototransistor so that the polarity of the collector is positive and that of the emitter is negative on condit...
...ight). A circuit to fully stabilize the power supply voltage is not built into the Sensors, and so the voltage supplied to the Sensors will fall when the LED is lit due to the cable resistanc...
...the negative terminal will not result in failure or other problems, but the product is designed so that the L terminal is open or connected to the positive terminal, so leave it open...
.../CJ-series Programmable Controllers are OFF. Other CPU Unit models do not have switch settings, so this does not need to be checked. When There Is a Power Supply Failure Check the power suppl...