| IAグローバル検索 |
...トメーションに最もシンプルな安全統合で安心・安全な生産現場を実現 NXシリーズ セーフティI/Oユニット NX-SI / SO シンプルで柔軟な安全システム構成を実現 ページ先頭へ戻る 生産終了品 生産終了品のカ...
...ase of the shutter. Easy filter replacement The light cover and optical filter are replaceable, so you don't need to prepare a protection cover against dirt. Single camera for inspecting vari...
... which allows multiple input voltage ranging 100 to 240 VAC. Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...
...oducts with safety outputs of which voltage, current, and power are limited to a certain level, so that not to cause an electric shock or fire,” and is evaluated by UL1310. For the UL Class 2...
...e the optical fiber, preventing stable detection. Easy Cable Routing The cable opening is wide, so the cable can be routed easily. Hex shape Provides Simplicity and Reliability Full lineup of...
... Optical Axis Accuracy The offset between the optical axis and mechanical axis is within ±2.5°, so a sufficient incident level can be achieved merely by aligning the mechanical axis at instal...
...ate of change of the heater resistance value and monitor the state and tendency of each heater, so it is possible to determine when replacement is necessary, so it is unplanned while...
...etup completed in just a few minutes Intuitive UI for effortless use The AI Detection Camera is so intuitive that even first-time users can set it up. Just follow the on-screen steps and conf...
...• The Configurator can be used to calibrate temperatures. • The circuit section can be removed, so rewiring isn’t required during maintenance. • DIN track mounting. last update: December 19, ...
...nd power factors to appropriate levels. Fixed values are used for the voltage and power factor, so the accuracy specifications do not apply. * Set the voltage to 100 V when performing simple ...
...egistration, RCM, cULus Simplicity improves reliability Unnecessary complexity causes problems, so we’ve eliminated it totally, to improve reliability, maximize performance. • No internal cab...
...egistration, RCM, cULus Simplicity improves reliability Unnecessary complexity causes problems, so we’ve eliminated it totally, to improve reliability, maximize performance. • No internal cab...
...ital Temperature Controller E5DC. July 4, 2013 We have introduced Safety Control Units NX-SL/SI/SO....
... which correspond to each slit, and is output as two square waves. The two slits are positioned so that the phase difference between the square wave outputs is 1/4 pitch. * Even if resolution...
...des. F03-15 Use this Sensing Band for dusty and humid environments. The electrodes are exposed, so install this Sensing Band in locations requiring insulated materials. F03-16PS F03-16PS-F Th...
... a Wide Area Ultrasonic Sensors detect reflection from a wider area than photoelectric sensors, so they can check a wide area all at the same time. 3. Non-Contact Detection Because Ultrasonic...
...reviously they could not go. Moreover, you can select a size according to the area of coverage, so targets are uniformly neutralized. Easy installation Ideal for narrow workbenches to wide li...
...t work properly. Performance Cookies These cookies allow us to count visits and traffic sources so that we can measure and improve the performance of our website. They help us to know which p...
...ustry. We are dedicated to empowering Indian businesses with the latest automation technologies so that they can optimise resource utilisation, minimize environmental impact, and make world-c...
...d regulations, OMRON will honour your request or objection, or inform you as to whether and, if so, to what extent it is complying therewith within 21 days or such other time as is reasonable...