Question
Please teach the principle of operation of Standard cylinder type Proximity Sensor the E2E Series.
Answer
The circuit composition and the principle of operation are as follows.
        1. Circuit composition
      
 
      
        2. Principle of operation
      
That is called the high frequency oscillation type, the eddy current is generated on the metal surface by the metal's approaching the oscillation coil built into sensing surface, and the impedance of the detector coil changes by the electromagnetic induction action.
As a result, the oscillation circuit that oscillates in the high frequency cannot oscillate and the oscillation level decreases.
The approach of the sensing object is detected depending on the decrease degree at this oscillation level.
 
      The eddy current is generated the higher the permeability of the sensing object like iron is, it is easy to for the sensor to detect it.
 
       E2E
E2E 
                    
                  Standard Sensors for Detecting Ferrous Metals under Standard Conditions
 What kind of consideration points does it have when the relay is connected to Proximity Sensors?
What kind of consideration points does it have when the relay is connected to Proximity Sensors?
                 What is the allowable bending radius of coaxial cables or shielded cables for Photoelectric Sensors and Proximity Sensors?
What is the allowable bending radius of coaxial cables or shielded cables for Photoelectric Sensors and Proximity Sensors?
                 How many 2-wire DC Proximity Sensors can be connected to the input side of B7AP Power Couplers?
How many 2-wire DC Proximity Sensors can be connected to the input side of B7AP Power Couplers?