Question
What are measures and malfunction mode when the relay of not being possible to connect it with the Proximity Sensor is connected?
Answer
Malfunction mode
1. The relay is not ON
When the proximity sensor does not meet the ON condition of the relay
2. The relay is not OFF
When the proximity sensor does not meet the OFF condition of the relay
3. The relay throbs
When the proximity sensor nearly meets the ON/OFF condition of the relay
Measures against malfunction
1. The relay is not ON
There are no measures.
2. The relay is not OFF or The relay throbs
Please put the bleeder resistance in parallel with the load. (Refer to the figure below.)
Standard Sensors for Detecting Ferrous Metals under Standard Conditions