Question
What is the current consumption for 2-wire DC Proximity Sensors?
Answer
For 2-wire DC Proximity Sensors, the current consumption is the same as the leakage current. The current consumption is 0.8 mA max. for the E2E-X[]D[] 2-wire DC Proximity Sensors.
 E2E
E2E 
                    
                  Standard Sensors for Detecting Ferrous Metals under Standard Conditions
 What kind of consideration points does it have when the relay is connected to Proximity Sensors?
What kind of consideration points does it have when the relay is connected to Proximity Sensors?
                 What is the allowable bending radius of coaxial cables or shielded cables for Photoelectric Sensors and Proximity Sensors?
What is the allowable bending radius of coaxial cables or shielded cables for Photoelectric Sensors and Proximity Sensors?
                 How many 2-wire DC Proximity Sensors can be connected to the input side of B7AP Power Couplers?
How many 2-wire DC Proximity Sensors can be connected to the input side of B7AP Power Couplers?