Question
Can a Photoelectric Sensor with an Optical Fiber be used in an explosion-proof area?
Answer
Everything except the Amplifier Unit can be used in an explosion-proof area.
Explanation:
A Photoelectric Sensor with an Optical Fiber has no electrical parts, and it can thus be used even in hazardous, explosion-proof areas. However, the lens, the case, and the fiber covering are made of plastic, so they must be free from corrosion or deterioration (fogging) due to contact with solvents.
As long fiber lengths are commonly used in explosion-proof areas, E32-T17L Fiber unit (standard fiber length: 10 m) is recommended.
 E2E
E2E 
                    
                  Standard Sensors for Detecting Ferrous Metals under Standard Conditions
 What's the difference between a Reflective Fiber Unit and a Coaxial Reflective Fiber Unit?
What's the difference between a Reflective Fiber Unit and a Coaxial Reflective Fiber Unit?
                 Our Photoelectric Sensors malfunction when the power supply of an inverter motor or other equipment is switched ON or OFF. 
What's causing this, and what can we do to resolve it?
Our Photoelectric Sensors malfunction when the power supply of an inverter motor or other equipment is switched ON or OFF. 
What's causing this, and what can we do to resolve it?
                 When using a Fiber Unit mounted to a movable part, are there models that are less affected by repetitive bending?
When using a Fiber Unit mounted to a movable part, are there models that are less affected by repetitive bending?