Question
The Reflector is fogged up. Is there any way to improve the situation?
Answer
Use E39-R1K Reflectors with a anti-fog coating. Regular Reflectors become fogged up when the temperature changes from -5°C to room temperature. Reflectors with anti-fog coating can withstand temperature changes from -25°C to room temperature.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions