Question
Can the Actuator's Measurement Head of D5V Contact Displacement Sensor be replaced?
Answer
The Actuator's Measurement Head of D5V cannot be replaced. The Flat Actuator, D5V[]-3F1, has an M2.5 screw so the Measurement Head can be replaced.
Models that have a replaceable Measurement Head are the D5SN-TN1, D5SN-TF1, and D5SN-TR1.
 E2E
E2E 
                    
                  Standard Sensors for Detecting Ferrous Metals under Standard Conditions
 Support Software "Smart Monitor" does not start properly. What is causing this, and what can be done to resolve it?
Support Software "Smart Monitor" does not start properly. What is causing this, and what can be done to resolve it?
                 Does the temperature of the sensing object affect the detection ability of E4PA Ultra Sonic Displacement Sensor?
Does the temperature of the sensing object affect the detection ability of E4PA Ultra Sonic Displacement Sensor?
                 When a command was sent using Z300 High-precision Laser Profiling System serial communications output, an error was returned. Why is this?
When a command was sent using Z300 High-precision Laser Profiling System serial communications output, an error was returned. Why is this?