Page top

Lead Contents

FAQ03425 of Displacement Sensors / Measurement Sensors FAQ

FAQ No. FAQ03425

Primary Contents

Question

Is the setting for the number of samples to average used for the linear output?

Answer



Yes, it is. When the number of samples to average is set, the measurement values are averaged, and the value is displayed on the Amplifier Unit and sent to the linear output.

Averaging is performed using a moving average.

Applicable models: ZX-L-N Smart Sensors, ZX-E Smart Sensors, and ZX-T Series Smart Sensors