Page top

Lead Contents

FAQ02265 of IT Products and Software Components FAQ

FAQ No. FAQ02265

Primary Contents

Question

Can multiple Programmable Controllers be connected to one PLC Reporter?

Answer



Yes. The maximum number depends on the network, but 32 Programmable Controllers from number 0 to number 32 can be connected for each communications port if Host Link is used.

Caution is required, however, because the communications time will increase as the number of Programmable Controllers connected increases.