Page top

Lead Contents

FAQ02531 of IT Products and Software Components FAQ

FAQ No. FAQ02531

Primary Contents

Question

Can the PLC Reporter 32 be connected to the peripheral port of a Programmable Controller?

Answer



PLC Reporter 32 supports communications in Host Link mode. The peripheral port is typically used for connection with a Programmable Controller or the CX-Programmer FA Integrated Tool Package in peripheral bus (toolbus) mode, but it can be used in Host Link mode. (Some of the old models do not support the Host Link mode.)

Settings vary with the Programmable Controller, so refer to the corresponding Programmable Controller manual.