Page top
Global
Global Navigation
Lead Contents
FAQ No. FAQ02532
Related Contents
Primary Contents
Question
What is the maximum data communications size of the PLC Reporter 32?
Answer
A maximum of 9,999 cells can be set up for data communications using the PLC Reporter 32. Allocating one word per cell, this equates to 9,999 words of data.
Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Port.
Package PLCs with Exceptional Cost
Motion, Logic and Vision in one
Local Navigation