Page top

Lead Contents

FAQ02546 of IT Products and Software Components FAQ

FAQ No. FAQ02546

Primary Contents

Question

Which Programmable Controllers can be connected with PLC Reporter 32?

Answer



In Host Link mode, any Programmable Controller that supports the Host Link mode can be connected.

For the multi-network version, any Programmable Controller that can interpret FINS commands can be connected. For details, check the manual of the Programmable Controller to be connected.

Different versions of PLC Reporter 32 are compatible with different Programmable Controllers. Once a Programmable Controller is set up for use, the parameters that can be modified are limited by that model. If the Programmable Controller that you want to connect is not listed within the PLC Reporter 32, select a model that has similar memory areas.