Primary Contents

IA Global Search Results

Select Country in

Site Search Product Search IA Global Search
Results 581 - 600 of 26275
FAQ02189 for Basic Switches | OMRON Industrial Aut...

...he case and cover, and in Switches. Resistant to gas. The terminal section is exposed, however, so caution is required for water and oil. D2JW Model with Terminals D2SW Model with Terminals D...

https://www.ia.omron.com/support/faq/answer/29/faq02189/

FAQ02231 for Basic Switches | OMRON Industrial Aut...

...gh switching speed shortens the time arcing is maintained. Contact wear and damage are reduced, so stable characteristics can be obtained. Large-capacity switching can be performed with compa...

https://www.ia.omron.com/support/faq/answer/29/faq02231/

faq02946

...gure shows, the Actuator fulcrum is in a different position from that of the standard Switches, so the internal movement is reversed. Even in the free position, the pin plunger is continuousl...

https://www.ia.omron.com/support/faq/answer/29/faq02946/

faq03149

...ches available? Answer  There is no definition of high-humidity processing for Basic Switches, so OMRON does not make such switches. Use standard models. 61F-G[]N Improved Design for a More ...

https://www.ia.omron.com/support/faq/answer/29/faq03149/

FAQ03331 for Basic Switches | OMRON Industrial Aut...

...rotary-action operation. Special-purpose Basic Switches are designed for specific applications, so they are limited to use, for example, as power switches for doors. Next, select the maximum ...

https://www.ia.omron.com/support/faq/answer/29/faq03331/

FAQ02105 for Limit Switches | OMRON Industrial Aut...

...tents FAQ No. FAQ02105 Related Contents Primary Contents Question Can WLNJ Limit Switch be used so that a bent coil spring becomes straight after striking the dog? Answer  Do not use the WLN...

https://www.ia.omron.com/support/faq/answer/30/faq02105/

faq02122

...is grounded? Answer  No, it must be grounded. The socket unit and the lead wire are insulated, so the lead wires must be grounded. 61F-G[]N Improved Design for a More Lightweight Constructio...

https://www.ia.omron.com/support/faq/answer/30/faq02122/

faq02149

...r to be caught or accumulate. WLNJ-30: The coil spring consists of three tightly wrapped wires, so there is almost no flexibility in the rod. Also, no gaps form in the coil spring. Reference ...

https://www.ia.omron.com/support/faq/answer/30/faq02149/

faq02990

... OF for a WLH12 with a roller lever length of 38 mm is 9.81 N (the OF listed in the datasheet), so the fixed torque is calculated as OF x R. Dividing this by R' (89 mm in this example), which...

https://www.ia.omron.com/support/faq/answer/30/faq02990/

FAQ00692 for Level Switches | OMRON Industrial Aut...

...d with a utility knife. Leave the insulation intact on the inside. (b)Strip back the insulation so that the enough wire is exposed to fit into the sleeve in the configuration shown in Figure ...

https://www.ia.omron.com/support/faq/answer/33/faq00692/

FAQ00702 for Level Switches | OMRON Industrial Aut...

...uch as fine sandpaper. Use a cloth to wipe off the residue. The electrodes are stainless steel, so it is also acceptable to use a commercial chemical cleanser, but be sure that the liquid in ...

https://www.ia.omron.com/support/faq/answer/33/faq00702/

FAQ00704 for Level Switches | OMRON Industrial Aut...

... Detector? Answer  Yes, it can be used, but it has different surge resistance characteristics, so do not use it in locations where it may be subjected to impulse surges, such as an outdoor r...

https://www.ia.omron.com/support/faq/answer/33/faq00704/

FAQ00709 for Level Switches | OMRON Industrial Aut...

...oller. Even if the rising water submerges E2, the resistance will be 6.8 kΩ + 3.9 kΩ = 10.7 kΩ, so the Controller's circuit will not operate. If the water reaches E1, the resistance will be o...

https://www.ia.omron.com/support/faq/answer/33/faq00709/

faq00716

... the Electrode Band into the lower hold of the connecting nut, and tighten the two clamp screws so that the conductor in the Electrode Band will come into contact with the connecting nut. The...

https://www.ia.omron.com/support/faq/answer/33/faq00716/

faq00730

...ternate Operation Relays to 61F-APN2? Answer  61F-APN and 61F-APN2 differ in outer dimensions, so the compatible Sockets and the mounting method will be different. This means that the Socket...

https://www.ia.omron.com/support/faq/answer/33/faq00730/

faq00735

...ectrodes. F03-14 1P is a one-pole type and there are no restrictions on its mounting intervals, so any Electrode Holder can be used. F03-14 3P and F03-14 5P can be used only with PS-[]S Elect...

https://www.ia.omron.com/support/faq/answer/33/faq00735/

faq00736

...l Controllers to substitute 61F-GP-N8? Answer  61F-GP-N8 and 61F-GP differ in outer dimensions so the compatible Sockets and the mounting method will be different. This means that the Socket...

https://www.ia.omron.com/support/faq/answer/33/faq00736/

FAQ00738 for Level Switches | OMRON Industrial Aut...

...stance includes the wiring from the 61F Controller's inputs (electrodes) to the 61F Controller, so the two values are not necessarily the same when there is a long distance, but generally the...

https://www.ia.omron.com/support/faq/answer/33/faq00738/

FAQ00751 for Level Switches | OMRON Industrial Aut...

...through the electrodes. If the electrodes are usually submerged, galvanic corrosion will occur, so the Ultra High-sensitivity model cannot be used for control. Applications are restricted to ...

https://www.ia.omron.com/support/faq/answer/33/faq00751/

faq00755

...swer  Electrodes are sold in 1-m increments. Electrode (F03-01) There are threads at both ends so it can be cut in half and used as two Electrodes. The threads (M6) have been created by roll...

https://www.ia.omron.com/support/faq/answer/33/faq00755/

Results 581 - 600 of 26275

Select Country in