| IAグローバル検索 |
...t applied. Applicable models: F3SN Series Safety Light Curtain F3SH Series Safety Light Curtain F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
... by making the protective height and sensor length the same, as shown in the following diagram. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...position). F3SN-A[][][][]P14 (Optical axis pitch: 9 mm, Smallest detectable object: 14 mm dia.) F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
... Contacts that are normally closed. Symbol NO Contacts: Contacts that are normally open. Symbol F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...are available? Answer Refer to the following address. http://www.ia.omron.com/product/26.html F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...rrupted. Applicable models: F3SN Series Safety Light Curtains F3SH Series Safety Light Curtains F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...systems in categories B, 1, and 2. Type-4 Safety Light Curtains can be used for all categories. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...ety function operates if the wiring is damaged and a short-circuit occurs between the channels. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...uits of the Safety Relay Unit "G9S-301" (excerpt) K1,K2,K3: Safety Relay built into the G9S-301 F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...estart thanks to this circuit, thus ensuring safety. However, be sure to use double contactors. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
... to using a manual reset for G9SA Safety Relay Units in Auto Reset Mode: Never use manual mode. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
... Contacts that are normally closed. Symbol NO Contacts: Contacts that are normally open. Symbol F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...d to a loss of the safety function. For this reason, the Safety Relay Unit requires two inputs. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...s the Safety Relay with other components in order for the safety circuit to be easily designed. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...not use this input method because it cannot detect faults, and it cannot ensure safe operation. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...is reason, Programmable Controller or Programmable Terminal cannot be used for safety circuits. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...acts) have the mark(*) on the nameplate. Forcibly Guided Contact Mechanism (G7SA Safety Relays) F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...nstalled upside down or to a position horizontal with the floor surface, no malfunction occurs. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
... to 4 in the figure) and the key can be inserted at eight points (points 1 to 8 in the figure). F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...
...cator terminals for D4DL Safety-door Switches and D4BL have polarity? Answer No, they do not. F3SR-B For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Gl...